This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:pmd-ard-intz [04 Sep 2020 08:50] – [I²C Port] Jesse Daniel Santos | resources:eval:user-guides:pmd-ard-intz [09 Mar 2023 03:21] (current) – updated the design files download link Joyce Velasco | ||
---|---|---|---|
Line 94: | Line 94: | ||
==== UART Port ==== | ==== UART Port ==== | ||
- | Pmod port (P13) can be reconfigured between an expanded SPI and expanded UART. To configure P13 as expanded UART, set the shunt connectors P8, P9, and P10 similiar to the encircled in Figure U. | + | Pmod port (P13) can be reconfigured between an expanded SPI and expanded UART. To configure P13 as expanded UART, set the shunt connectors P8, P9, and P10. |
^Pin No.^P13: UART^ | ^Pin No.^P13: UART^ | ||
Line 117: | Line 117: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | **PMD-ARD-INTZ Design & Integration Files** | + | [[adi> |
- | * {{: | + | |
- | * {{: | + | * PCB Layout |
- | * {{: | + | * Bill of Materials |
+ | * Allegro Project | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |