This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:pmd-ard-intz [18 Aug 2020 05:50] – [Schematic, PCB Layout, Bill of Materials] Jesse Daniel Santos | resources:eval:user-guides:pmd-ard-intz [09 Mar 2023 03:21] (current) – updated the design files download link Joyce Velasco | ||
---|---|---|---|
Line 5: | Line 5: | ||
{{: | {{: | ||
- | **REPLACE WITH NEW REV BOARD** | ||
- | ---- | ||
===== General Setup ===== | ===== General Setup ===== | ||
Line 22: | Line 20: | ||
{{: | {{: | ||
- | **REPLACE WITH NEW REV BOARD** | + | |
==== Logic Voltage Settings ==== | ==== Logic Voltage Settings ==== | ||
Line 34: | Line 32: | ||
{{: | {{: | ||
- | **REPLACE WITH NEW REV BOARD** | + | |
Meanwhile, the logic voltage source of the MCU baseboard can be chosen from the IOREF from the MCU baseboard header and the 3.3V and 5V system voltages using the shunt connector between P22 and P21 (encircled blue in Fig D). Preferably, this should be set to IOREF to ensure a proper voltage setting. | Meanwhile, the logic voltage source of the MCU baseboard can be chosen from the IOREF from the MCU baseboard header and the 3.3V and 5V system voltages using the shunt connector between P22 and P21 (encircled blue in Fig D). Preferably, this should be set to IOREF to ensure a proper voltage setting. | ||
Line 45: | Line 43: | ||
{{: | {{: | ||
- | **REPLACE WITH NEW REV BOARD** | ||
- | ---- | ||
- | |||
===== Pmod Interface Types ===== | ===== Pmod Interface Types ===== | ||
Line 95: | Line 90: | ||
{{: | {{: | ||
- | **REPLACE WITH NEW REV BOARD** | + | |
==== UART Port ==== | ==== UART Port ==== | ||
- | Pmod port (P13) can be reconfigured between an expanded SPI and expanded UART. To configure P13 as expanded UART, set the shunt connectors P8, P9, and P10 similiar to the encircled in Figure U. | + | Pmod port (P13) can be reconfigured between an expanded SPI and expanded UART. To configure P13 as expanded UART, set the shunt connectors P8, P9, and P10. |
^Pin No.^P13: UART^ | ^Pin No.^P13: UART^ | ||
Line 122: | Line 117: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | PMD-ARD-INTZ Design & Integration Files | + | [[adi> |
- | * {{: | + | * Schematic |
- | * {{: | + | * PCB Layout |
- | * {{: | + | * Bill of Materials |
+ | * Allegro Project | ||
</ | </ | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | |||
+ | // End of document // |