This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision Last revision Both sides next revision | ||
resources:eval:user-guides:pioneer1-wiredcbm [15 Feb 2021 16:36] Richard Anslow [Change Log] |
resources:eval:user-guides:pioneer1-wiredcbm [15 Feb 2021 16:42] Richard Anslow [Change Log] |
||
---|---|---|---|
Line 168: | Line 168: | ||
When simulating Figure 10 it is also worth noting that the C8 capacitor is recommended to reduce voltage overshoot at the sensor (Vpout at power extraction node). With C8 added the overshoot is maximum 47mV and settles to within 1mV of the desired 5VDC within 1.6ms. Simulating without a C8 capacitor results in an underdamped system, with 600mV overshoot, and a permanent 100mV of voltage oscillation from the 5V dc target. | When simulating Figure 10 it is also worth noting that the C8 capacitor is recommended to reduce voltage overshoot at the sensor (Vpout at power extraction node). With C8 added the overshoot is maximum 47mV and settles to within 1mV of the desired 5VDC within 1.6ms. Simulating without a C8 capacitor results in an underdamped system, with 600mV overshoot, and a permanent 100mV of voltage oscillation from the 5V dc target. | ||
+ | LTSpice models are available here: | ||
+ | {{ :resources:eval:user-guides:podl_article.zip |click here to download}} | ||
===== Change Log ===== | ===== Change Log ===== | ||
*July 2019. Initial Release. | *July 2019. Initial Release. | ||
+ | |||
*August 2019. Added additional information on demo power supply configuration. | *August 2019. Added additional information on demo power supply configuration. | ||
+ | |||
*February 2021. Added LTspice models for engineered power. | *February 2021. Added LTspice models for engineered power. | ||