Wiki

This version (09 Nov 2023 02:09) was approved by Zuedmar Arceo.

Power Amplifier (PA) Array Controller User Guide

Overview

The optimal performance of RF power amplifiers depends on precise biasing control, which enhances factors like linearity and efficiency. GaN HEMTs have proven superior in high-frequency and high-power RF applications but require careful bias voltage timing to prevent device damage. To ensure safe and reliable operation, proper biasing sequence and protection are essential. This reference design utilizes ADI’s portfolio for control, protection, and appropriate bias sequencing of RF power amplifier arrays designed for massive MIMO and macro base-station applications. The system manages the power-up and power-down progression of Power Amplifier arrays while continuously monitoring the system’s crucial parameters.

block_diagram.jpg Figure 1. System Architecture

The conventional approach of powering up and powering down of GaN amplifiers involves using multiple bench power supplies and manually turning them on and off based on the specific amplifier requirements. However, this method carries a high risk of damaging the amplifier due to potential human errors and is neither time-efficient nor cost-effective.

The PA Array Board reference design helps address these challenges, this innovative reference design eliminates human errors and fully automates the power-up and power-down procedure, ensuring the safe and reliable operation of GaN amplifiers.

Features

  • Fault Event Protection -- undervoltage, overvoltage,overcurrent, overtemperature.
  • Fast GaN gate voltages settling time ~ <5 microseconds
  • Fast fault event to gate pinch-off time ~ <10 microseconds
  • Wide range of gate bias voltages +/- 10V
  • Precise power-up and down sequence of up to two GaN HEMTs-based amplifier

Applications

  • 5G massive MIMOs
  • Macro base-stations

Reference Design Hardware

Primary Side

hw_top_label.jpg Figure 2. Top View

Power Supply Connectors

power_input.jpg

  • These connectors are used to supply +48V to the entire circuitry. The PA Array Controller Board provides an option for the user to use either a barrel jack connector or a two-wire terminal.
    • P1 is a power barrel connector jack. The user can use this port if they have a +48V barrel jack.
    • P2 is a two-port terminal connector. Any bench power supply can use this port. Make sure to properly connect the positive and negative terminals of the power supply.
  • The user can choose either of the two power supply connectors, P1 or P2. Note that using these two connectors at the same time is not recommended and can incur damage to the board.

LED Indicators

led.jpg

  • The reference design uses four LEDs to indicate its current status:
    • DS1 LED indicates that there is a fault event occurring on the first GaN amplifier.
    • DS2 LED indicates that there is a fault event occurring on the pre-driver and driver amplifiers.
    • DS3 LED indicates normal operation and good power regulation.
    • DS4 LED indicates that there is a fault event occurring on the second GaN amplifier.

Peripheral Connectors

peripherals.jpg

  • These connectors are used for debugging, programming, and communication between the software and hardware.
    • P5USB UART-SERIAL Communication
    • P6 → SWD Debugger

Switches

switch.jpg

  • The main purpose of the switches is to reset a certain device:
    • S1 → LTC7000_1 Reset
    • S2 → LTC7000_2 Reset
    • S3 → MAX32666 Microcontroller Reset
    • S4 → LTC7000_3 Reset

Test Points

  • The reference design board is composed of several test points. The table below describes some of the most significant test points and their descriptions.

test_points.jpg

Test Points
TP Name Description Voltage
TP3 U1 LTC7000_1 Output +48V
TP6 U2 LTC7000_2 Output +48V
TP22 U25 LTC7000_3 Output +48V
TP11 U6 MAX17643 Output +5.6V
TP15 U10 LT3471 Positive Output +12V
TP16 U10 LT3471 Negative Output -12V
TP8 U3 ADM7172 LDO Output +5V
TP10 U5 LT3042 LDO Output +5V
TP9 U4 LT3042 LDO Output +5V
TP14 U9 ADM7150 LDO Output +5V
TP13 U8 ADM7170 LDOOutput +1.8V
TP12 U7 ADM7170 LDO Output +3.3V
TP17 U11 ADP161 LDO Output +1.1V

Pin Turrets and Hooks

  • The PA Array Controler Board was designed for specific power amplifiers and is used on the RF signal chain as shown below.

Figure 3. RF Signal Chain

  • The bias lines of these amplifiers must be connected to their desired pinouts on the reference design board. Refer to the table below for the correct pin assignments.

Pin Assignments
Pin Name Description Pin Type
5V0_802 HMC802A VDD Pin Hook
EN_802 HMC802A Enable Pin Hook
5V0_PDA ADL5611 VPOS Pin Hook
5V0_DA BTS6201U VCC Pin Hook
EN_DA BTS6201U Enable Pin Hook
VDC1 A5M36TG140 LDMOS Carrier Drain Pin Hook
VDP1 A5M36TG140 LDMOS Peaking Drain Pin Hook
VGC1 A5M36TG140 LDMOS Carrier Gate Pin Hook
VGP1 A5M36TG140 LDMOS Peaking Gate Pin Hook
VDC2 A5M36TG140 GaN Carrier Drain Pin Turret
VDP2 A5M36TG140 GaN Peaking Drain Pin Turret
VGC2 A5M36TG140 GaN Carrier Gate Pin Hook
VGP2 A5M36TG140 GaN Peaking Gate Pin Hook
VD1 GTRB384608FC-V1 GaN Main Drain Pin Turret
VD2 GTRB384608FC-V1 GaN Peak Drain Pin Turret
VG1 GTRB384608FC-V1 GaN Main Gate Pin Hook
VG2 GTRB384608FC-V1 GaN Peak Gate Pin Hook

Secondary Side

Figure 4. Bottom View


System Setup

Note that this user guide only allows the user to test and measure the time transition of the following:

  • AD3552R DAC settling time
    • From pinch-off to normal operating voltage
    • From normal operating to pinch-off voltage
  • Fault detection up to DAC pinch-off voltage

The PA Array Controller Board was not fully characterized so this user guide only test and measure the settling time of the three DACs and fault detection.

Requirements

The following is the list of items needed to replicate the timing test.

Hardware

  • PA Array Controller Board
  • One (1) Programmable Power Supply.
    • It should accommodate a voltage level of +30V to +60V.
  • Two (2) micro-USB to USB cable.
    • For UART-Serial communication
    • For SWD Debugger
  • One (1)MAX32625-PICO with SWD cable
  • One (1) 4-channel oscilloscope
  • One (1) Oscilloscope probe
  • Six (6) 10nF capacitors - act as a load for all 6 Gate pins

Warning: The PA Array Controller Board was not fully characterized yet. So, we do not recommend using the actual amplifiers as a load, but instead, use a 10 nF capacitor.

Firmware

  • To properly load the firmware onto the board, simply drag and drop the provided .hex file to the DAPLINK drive. Using the drag-and-drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design.

General Test Setup

This section describes the basic setup and connections in order for the user to bring up the board.

Hardware Setup

Figure 5. Setting up the hardware

  1. First, connect the 10-pin SWD debug cable to port P6 of the PA Array Board.
  2. Next is to connect the other end of the SWD debug cable to the MAX32625 Pico.
  3. Use the micro-USB to USB cable to connect the MAX32625 Pico to your PC/Laptop. This connection allows the user to upload firmware to the board.
  4. Then, connect the other micro-USB to USB cable to port P5. This connection allows the USB-UART communication that enables the user to access the Graphical User Interface (GUI).
  5. From your PC, open My Computer and look for the DAPLINK drive, if you see this then the drivers are complete and correct. Figure 6. DAPLINK Drive
  6. Connect the positive terminal of the +48V Power Supply to port P2.1.
  7. Then, connect the negative terminal to port P2.2. Do not turn-on the power supply yet.
  8. Lastly, connect the osc probe to the oscilloscope.

Software Setup

  1. The board has already been pre-loaded with firmware v0.0.10112023[BETA]P0_21.
  2. If the user would like to re-upload the firmware again, simply drag and drop the provided ADI PA Array Firmware v0.0.10112023[BETA] (.hex) file onto the DAPLINNK drive.
  3. To access the graphical user interface (GUI), open the provided PA Array UI (.exe) file. For a better understanding of the GUI's functionality and features, please refer to the image provided below, which offers a concise description of the graphical user interface.

Figure 7. Dashboard

Figure 8. Monitor and Control Panel

Figure 9. GUI Overview Figure 10. GUI Historical Graph Figure 11. GUI Device Group Figure 12. GUI Control Group

Basic Operation

  • Now that we are finished setting up the hardware and firmware. We will begin to measure the timing response of each AD3552R DAC's.
  1. Let's start to measure the settling time of the DAC on the GaN gate pins (VGC2, VGP2, VG1, VG2).
  2. Connect a 10nF capacitive load on each GAN gate pins (VGC2, VGP2, VG1, VG2) pin with respect to ground.
  3. The positive and negative terminals of all channels of the oscilloscope probe must connect in parallel to each of the capacitor pins.
  4. Now, set the required configurations of the oscilloscope:
    • -3V on rising edge trigger value.
    • 1us/div and 2V/div.
  5. Refer to Figure 5 for the complete hardware setup.
  6. Upon board boot-up, the default voltages on the GaN gate pins are the pinch-off voltages (-5V).
  7. On the GUI, the user has the freedom to choose any voltage they desire from -10V to +10V range. For our example, let's set all the carrier and peak gates to their corresponding operating voltages.
    1. VGC2: -2V
    2. VGP2: -2.6V
    3. VG1: -2.75V
    4. VG2: -2.75V
  8. There are two ways to set the voltages. The first is by using the spin box and the second is by using the slider. Figure 7. Setting the GaN gate voltages through GUI
  9. Once the voltages are entered, press the set button. Do this process on each of the GaN gates to replicate the oscilloscope result.
  10. You will see the voltage translation from pinch-off to operating voltage. The oscilloscope will display the voltage transition and the time response. The result should be the same as the images below. Figure 7. VGC2 Voltage Time Response Figure 8. VGP2 Voltage Time Response Figure 9. VG1 Voltage Time Response Figure 10. VG2 Voltage Time Response
  11. Let's measure this time the DAC voltage transition of the LDMOS gate pins (VGC1, VGP1).
  12. Connect a 10nF capacitive load on each LDMOS gate pins (VGC1, VGP1) pin with respect to ground.
  13. The positive and negative terminals of the oscilloscope probe must connect in parallel to each of the capacitor pins.
  14. Adjust oscilloscope settings:
    • Trigger value: +1V on rising edge
  15. The default voltages of the LDMOS gate pins are pinch-off voltages (0V). Set the gate to its operating voltages.
    • VGC1: +3.8V
    • VGP1: +1.9V Figure 7. Setting the LDMOS gate voltages through GUI
  16. Once the voltages are entered, press the set button. You will see the voltage translation from pinch-off to operating voltage. The oscilloscope will display the voltage transition and the time response. The result should be the same as the images below. Figure 11. VGC1 Voltage Time Response Figure 12. VGP1 Voltage Time Response
  17. At this point, all the gate pins are in the normal operating voltage state. We are now ready to measure the voltage transition from normal operating to pinch-off voltage.
  18. Connect all 4-channels of the oscilloscope probes in parallel with all the capacitor pins.
  19. Adjust oscilloscope settings:
    • Trigger value: -3V on falling edge
  20. Set the gate voltages to their pinch-off voltages.
    • VGC2: -5V
    • VGP2: -5V
    • VGC1: 0V
    • VGP1: 0V
    • VG1: -5V
    • VG2: -5V Figure 7. Setting the GaN gate voltages through GUI
  21. Press the set button to reflect the changes. The result should be the same as the image below. Figure 13. VGC2 Voltage Time Response Figure 14. VGP2 Voltage Time Response Figure 15. VG1 Voltage Time Response Figure 16. VG2 Voltage Time Response Figure 17. VGC1 Voltage Time Response Figure 18. VGP1 Voltage Time Response

    Please note that the capacitor value used in the feedback loop of the trans-impedance amplifier is 100 pF. The relationship between speed and oscillation ripple is inversely proportional. We can achieve a faster settling time but must sacrifice a much cleaner oscillation, and vice versa.

  22. We are done capturing the voltage transition from power-up and power-down. Now, we will capture the time it takes from when the fault is detected until the DAC outputs the gate pinch-off voltage.
  23. We have already gathered data from the fault protection circuit, LTC7000. When it detects a fault event, it sends a signal from LTC7000 to the MCU in approximately 1 microsecond. This value will then be added to the system power-down measurement and the time it takes for the MCU to process the fault flag up to the DAC command. Figure 19. LTC7000 → MCU GPIO Fault Flag Time
  24. Follow the below steps:
  25. Place the positive terminal of the oscilloscope probe into the provided wire as shown in the image below. Then connect the negative terminal of the oscilloscope probe to the GND of the board. Figure 20. Fault Detection Time Measurement Setup
  26. Set the required oscilloscope settings.
    • Trigger value: +1V
    • 1us/div and 1V/div
  27. For this test, we will introduce an overvoltage fault. To do this, increase the voltage from the external power supply from +48V to +56V. This will cause a fault event since the preset threshold for an overvoltage is +55V.
  28. The oscilloscope will display a similar time response as shown below. Figure 21. MCU Processing Time
  29. On the GUI, it will notify the user that a fault event occurred and show a warning message as in the image below. Figure 21. Warning Message
  30. Also, the GUI is capable of logging and displaying the fault event time and on which device it occurs. Figure 21. Fault Logging
  31. The overall time from LTC7000 fault detection up to the DAC pinch-off voltage is shown on the Fault Event Time Summary below.

Summary of Results

System Power Up and System Power Down Summary

  • The below table shows the summary of our time response test for each DAC's. As shown below, we achieved the <5us time requirement.
Timing Response
Pin Name Description Pinch-off voltage (V) Operating Voltage (V) Power-up time (us) Power-down time (us)
VGC1 A5M36TG140 LDMOS Carrier Gate 0 +3.8 2.09 2.25
VGP1 A5M36TG140 LDMOS Peaking Gate 0 +1.9 1.65 2.01
VGC2 A5M36TG140 GaN Carrier Gate -5 -2 1.95 2.05
VGP2 A5M36TG140 GaN Peaking Gate -5 -2.6 1.73 1.95
VG1 GTRB384608FC-V1 GaN Main Gate -5 -2.75 1.81 2.00
VG2 GTRB384608FC-V1 GaN Peak Gate -5 -2.75 1.81 2.00

Table 1. Gate Voltages Timing response Summary

  • Power-up time → from pinch-off voltage to operating voltage.
  • Power-down time → from operating voltage to pinch-off voltage.

Fault Event Time Response Summary

  • The below table shows the summary of our time response test when a fault occurs. As shown below, we achieved the <10us time requirement.
  • The total time from fault detection up to the gate pinch-off is given by:
    • Total time = Fault flag (us) + MCU Processing time (us) + RF switch time (us) + highest power down time between VGC2, VGP2,VG1,VG2 (us) + highest power down time between VGC1, VGP1
    • Total time = 1.0898 us + 3.7078 us + 0.3 us + 2.05 us + 2.25 us
    • Total time = 9.4 us

Fault flag time → time it takes for the MCU to recognize that there is a fault signal coming from the LTC7000.

MCU processing time → total time for MCU to process the fault flag signal up to commanding the DAC.

RF switch time → total time for the RF switch to turn-off

Power-down time → DAC output from operating voltage to pinch-off.

Total time → time from fault detection to Vgg pinch-off


Miscellaneous Measurements

As per the customer's request, we are able to test and measure the DAC settling time from these specified voltage levels

  • Pinch-off voltage: -7V
  • Operating voltage: -1.2V

Do note that the firmware loaded on the board doesn't include these measurements. We can send a separate firmware if necessary.

-7V to -1.2V DAC Settling Time

The DAC output voltage settling time from -7V pinch-off to -1.2V is 2.31us. See the image below. Figure 22. -7V to -1.2V DAC Settling Time

-1.2V to -7V DAC Settling Time

The DAC output voltage settling time from -1.2V pinch-off to -2V is 2.31us. See the image below. Figure 23. -1.2V to -7V DAC Settling Time

End of Document

resources/eval/user-guides/pa-array-biasing-reference-design.txt · Last modified: 20 Oct 2023 11:25 by Zuedmar Arceo