Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:mykonos:software:filters [28 Aug 2017 08:47] – [Using the MATLAB App and Exe] sripad Jadhav | resources:eval:user-guides:mykonos:software:filters [17 May 2018 10:48] – [Use MATLAB App] sripad Jadhav |
---|
| |
* **Executable**: the executable includes the exe which allows the wizard to run as a separate application without requiring the MATLAB program to be running. The program provides a GUI that allows users to define the input parameters, generate filters, view the output results, and save all output parameters for their own use or use in the ADI EVB GUI software. To run this as a stand alone application, the MATLAB runtime engine needs to be installed (see link below). The runtime engine can take more than a minute to start up the first time it is run, so please be patient while it initializes. | * **Executable**: the executable includes the exe which allows the wizard to run as a separate application without requiring the MATLAB program to be running. The program provides a GUI that allows users to define the input parameters, generate filters, view the output results, and save all output parameters for their own use or use in the ADI EVB GUI software. To run this as a stand alone application, the MATLAB runtime engine needs to be installed (see link below). The runtime engine can take more than a minute to start up the first time it is run, so please be patient while it initializes. |
>> The MATLAB runtime engine can be downloaded from the following link: | The MATLAB runtime engine can be downloaded from the following link: |
[[https://www.mathworks.com/products/compiler/mcr.html]] | [[https://www.mathworks.com/products/compiler/mcr.html]] |
| |