Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:mykonos:software:filters [01 Aug 2017 13:23] – [Use MATLAB App] sripad Jadhav | resources:eval:user-guides:mykonos:software:filters [17 May 2018 10:48] – [Use MATLAB App] sripad Jadhav |
---|
There are three ways you can use the AD9371 Filter Wizard: | There are three ways you can use the AD9371 Filter Wizard: |
| |
* **Executable**: the executable includes the exe which allows the wizard to run as a separate application without requiring the MATLAB program to be running. To run this as a stand alone application matlab runtime needs to be installed, the required version is mentioned in release notes. It can take more than a minute for the runtime engine to start up for the first time so please be patient while it initializes. The program provides a GUI allowing users to define the input parameters, generate filters, view the output results, and save all output parameters for their own use or use in the ADI EVB GUI software. | * **Executable**: the executable includes the exe which allows the wizard to run as a separate application without requiring the MATLAB program to be running. The program provides a GUI that allows users to define the input parameters, generate filters, view the output results, and save all output parameters for their own use or use in the ADI EVB GUI software. To run this as a stand alone application, the MATLAB runtime engine needs to be installed (see link below). The runtime engine can take more than a minute to start up the first time it is run, so please be patient while it initializes. |
> Matlab runtime engine can be downloaded from below link | The MATLAB runtime engine can be downloaded from the following link: |
[[https://www.mathworks.com/products/compiler/mcr.html]] | [[https://www.mathworks.com/products/compiler/mcr.html]] |
| |
* **MATLAB App**: the App runs as an application within MATLAB and requires MATLAB to be running and licenses must exist for the Control System Toolbox as well as MATLAB itself. The GUI and flexibility are identical to the executable, but running as an app allows the user to write additional code to post process the existing matrices created by the wizard. | * **MATLAB App**: the app runs as an application within MATLAB. Use of the app requires MATLAB to be running with valid licenses for the Control System Toolbox as well as MATLAB itself. The GUI and flexibility are identical to the executable, but running as an app in MATLAB allows the user to write additional code to post-process the data files created by the wizard. |
* **MATLAB source code (function)**: These are MATLAB functions which users can launch from the MATLAB command window by properly defining the input parameters. Used this way, users have more control of the internal design process. | * **MATLAB source code (function)**: These are MATLAB functions which users can launch from the MATLAB command window by properly defining the input parameters. Used this way, users have more control of the internal design process. |
| |
[[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371 Filter Wizard.mlappinstall|App for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371 Filter Wizard.mlappinstall|App for Chrome/Firefox]] | [[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371 Filter Wizard.mlappinstall|App for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371 Filter Wizard.mlappinstall|App for Chrome/Firefox]] |
| |
The Source code is available here: | The source code is available here: |
[[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371FilterWizard_Source_v1.10.zip|Source for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371FilterWizard_Source_v1.10.zip|Source for Chrome/Firefox]] | [[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371FilterWizard_Source_v1.10.zip|Source for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371FilterWizard_Source_v1.10.zip|Source for Chrome/Firefox]] |
| |
| |
{{:resources:eval:user-guides:mykonos:software:tx_error_samplerate.jpg?300|}} | {{:resources:eval:user-guides:mykonos:software:tx_error_samplerate.jpg?300|}} |
| |
| When you click on the "Output Profile to Files" button, wizard generates four files as described below |
| |
| - <file_name>.txt - Used for configuring AD9371 in GUI and script generation |
| - <file_name>_AD9528.txt – Used for configuring AD9528 using TES GUI only, it will be generated if box is checked against "Write AD9528 settings to File" option. |
| - <file_name>_orxadc.txt – Used by GUI for plotting ORX ADC STF response only |
| - <file_name>_rxadc.txt - Used by GUI for plotting RX ADC STF response only |
| |
====== AD9371 Filter Wizard Rules ====== | ====== AD9371 Filter Wizard Rules ====== |