Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:mykonos:software:filters [14 Jan 2021 05:24] – use mw> interwiki links Robin Getzresources:eval:user-guides:mykonos:software:filters [05 Oct 2023 14:27] (current) – [Use MATLAB App] Michael Hennerich
Line 21: Line 21:
   * **MATLAB source code (function)**: These are MATLAB functions which users can launch from the MATLAB command window by properly defining the input parameters. Used this way, users have more control of the internal design process.    * **MATLAB source code (function)**: These are MATLAB functions which users can launch from the MATLAB command window by properly defining the input parameters. Used this way, users have more control of the internal design process. 
  
-The executable is available here: [[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371FilterWizard_EXE_v1.10.zip|exe for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371FilterWizard_EXE_v1.10.zip|exe for Chrome/Firefox]]+The executable is available here: 
 +[[ez>rf/wide-band-rf-transceivers/design-support-ad9371/w/documents/18048/ad9371-75-filter-wizard-setup-file-faq]]
  
-The app is available here: 
-[[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371 Filter Wizard.mlappinstall|App for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371 Filter Wizard.mlappinstall|App for Chrome/Firefox]] 
  
 The source code is available here: The source code is available here:
-[[ftp://adirfbwacust:67f1BoY@ftp.analog.com/users/adirfbwacust/AD9371_Filter_Wizard/AD9371FilterWizard_Source_v1.10.zip|Source for IE]][[ftp://adirfbwacust:67f1BoY@ftp.analog.com/AD9371_Filter_Wizard/AD9371FilterWizard_Source_v1.10.zip|Source for Chrome/Firefox]]+[[ez>rf/wide-band-rf-transceivers/design-support-ad9371/m/file-uploads/2924]]
  
 This section elaborates on the first two options, the executable and the App, and addresses both identically since the input and output functionality is the same.  This section elaborates on the first two options, the executable and the App, and addresses both identically since the input and output functionality is the same. 
resources/eval/user-guides/mykonos/software/filters.txt · Last modified: 05 Oct 2023 14:27 by Michael Hennerich