Wiki

This version is outdated by a newer approved version.DiffThis version (22 Aug 2019 10:05) was approved by Adrian Costina.The Previously approved version (09 Aug 2019 14:26) is available.Diff

This is an old revision of the document!


ADRV9371/PCBZ Quick Start Guides

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the ADRV9371-N/PCBZ, ADRV9371-W/PCBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported Carriers

The ADRV9371/PCBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

Board ADRV9371-N/PCBZ ADRV9371-W/PCBZ ADRV9375-N/PCBZ
ZCU102
KCU105
ZC706
Arria 10 SoC
Arria 10 GX

Supported Environments

The supported OS are:

Board HDL Linux Software No-OS Software
ZCU102
KCU105
ZC706
Arria 10 SoC
Arria 10 GX

Hardware Setup

In most carriers, the ADRV9371/PCBZ board connects to the HPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.

ZC706 + ADRV9371/PCBZ

ZCU102 + ADRV9371/PCBZ

Connect ADRV9371 into HPC0 on your ZCU102.

Unboxing guide

resources/eval/user-guides/mykonos/quickstart.1566461127.txt.gz · Last modified: 22 Aug 2019 10:05 by Adrian Costina