The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the ADRV9371-N/PCBZ, ADRV9371-W/PCBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.
The ADRV9371/PCBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:
Board | ADRV9371-N/PCBZ | ADRV9371-W/PCBZ | ADRV9375-N/PCBZ |
---|---|---|---|
ZCU102 | √ | √ | √ |
KCU105 | √ | √ | √ |
ZC706 | √ | √ | √ |
Arria 10 SoC | √ | √ | √ |
Arria 10 GX | √ | √ | √ |
The supported OS are:
Board | HDL | Linux Software | No-OS Software |
---|---|---|---|
ZCU102 | √ | √ | √ |
KCU105 | √ | √ | √ |
ZC706 | √ | √ | √ |
Arria 10 SoC | √ | √ | |
Arria 10 GX | √ | √ | √ |
In most carriers, the ADRV9371/PCBZ board connects to the HPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.
Connect ADRV9371 into HPC0 on your ZCU102.