This is an old revision of the document!
AD9371/AD9375 No-OS Setup
This guide provides some quick instructions on how to setup the AD9371 mykonos on:
Required Software
We're upgrade the Xilinx tools on every release. The supported version number can be found in our
git repository .
Some applications (
e.g. FMCOMMSx), when a Microblaze processor is used, requires an increased HEAP size for dynamic memory allocation. Make sure the HEAP size is at least
0x100000.
//#define XILINX
#define ALTERA
After the FPGA was programmed, we need to create a new Run configuration, by selecting Run → Run Configurations…, in the Run Configuration windows select the Xilinx C/C++ application (System Debugger) and click at the New Configuration button at the upper left corner.
If your target carrier has a Zync SoC, make sure, that you specify the Initialization file, and select the Run ps7_init and Run ps7_post_config options.
The output of the example program can be viewed in the SDK console by enabling the Connect STDIO Console option and setting the baud rate of the
UART port to 115200.
As an alternative a
UART terminal can be used to capture the output of the example program. The number of used
UART port depends on the computer's configuration. The following settings must be used in the
UART terminal:
Baud Rate: 115200bps
Data: 8 bit
Parity: None
Stop bits: 1 bit
Flow Control: none
Files
AD9371/AD9375 No-OS Software
-
Next copy the files intro the src folder of your newly created project. You can do this with Ctrl+C Ctrl+
V or simple drag and drop
-
-
Unzip the archive and go into src→api folder
Next copy the ad9528 and mykonos folder to the src folder of your project. Do NOT copy the common.c and common.h files provided by the api. For now, use the ones downloaded from github.
Make sure the paths for the directories are included. Right click on the src folder from Project Explorer and go to Properties → C/C++ Build → Settings → ARM v7 gcc compiler → Directories
Note: The AD9371/AD9375 evaluation board contains an on-board voltage controlled crystal oscillator (VCXO), there are limitations with the default hardware configuration in the scenario where user desired device frequencies are not related to the on-board 122.88
MHz VCXO by a rational fraction.
Push data into/out of the AD9371/AD9375
Below is defined the dac_core structures used by the dac_setup() and dac_write_custom_data() functions:
typedef struct
{
uint32_t base_address;
uint8_t resolution;
dac_channel *channels;
uint32_t dac_ddr_baseaddr;
}dac_core;
typedef struct
{
uint32_t dds_frequency_tone0; // in hz (1000*1000 for MHz);
uint32_t dds_phase_tone0; // in milli(?) angles (90*1000 for 90 degrees = pi/2)
int32_t dds_scale_tone0; // in micro units (1.0*1000*1000 is 1.0)
uint32_t dds_frequency_tone1; // in hz (1000*1000 for MHz)
uint32_t dds_phase_tone1; // in milli(?) angles (90*1000 for 90 degrees = pi/2)
int32_t dds_scale_tone1; // in micro units (1.0*1000*1000 is 1.0)
uint32_t dds_dual_tone; // if using single tone for this channel, set to 0x0
uint32_t pat_data; // if using SED/debug that sort of thing
dac_data_src sel; // set to one of the enumerated type above.
}dac_channel;
Below is defined the adc_core structure used by the adc_setup() and adc_capture() functions:
typedef struct
{
uint32_t base_address;
uint8_t master;
uint8_t no_of_channels;
uint8_t resolution;
uint32_t start_address;
}adc_core;
DDS Mode
DMA Mode
Set dac_data_src to
DAC_SRC_DMA.
dac_write_custom_data() function takes as argument the sine_lut_iq array which contains the custom data to be transmitted.
The format for each I and Q is 16-bit signed two's complement. I and Q together make up one 32-bit tx sample.
Capture data
Once DDS or
DMA mode is selected and the project configuration can be ran.
Open an
UART terminal, set the baud rate to 115200bps and make sure the initialization was completed, as in the screenshot bellow:
-
capture.bat script contains the path of the Xilinx SDK, the default is “C:\Xilinx\SDK\$VERSION”; if on your PC the path is different, you need to update it according to your project setup.
By running capture.bat, the iq_rx1.csv and iq_rx2.csv files will be generated.
Start
VisualAnalog and open the
visual_analog.vac file downloaded from the git repository.
From the Pattern Loader window, browse for the newly generated .csv files and click Run. The result should look something like in the screenshot below:
This guide provides some quick instructions on how to setup the AD9371 mykonos on:
Required Software
Altera Software setup
This section is intended to give a briefly review about how the user can make a new application project for his or her hdl design. If you are an advanced user, you probably want to skip this section.
Before the image can be loaded the Quartus Prime 16.0 tool or the Quartus Prime 16.0 Programmer must be installed on your computer.
The first step before get started is to
build the desired HDL design.
Open the NIOS II Software Build Tools for Eclipse. When NIOS II starts it asks to provide a folder, where to store the work space. Any folder can be provided.
Go to
File → New → NIOS II Board Support Package
Browse for the
SOPC Information File:
Type a
Project name and click
Finish:
Go to
File → New → NIOS II Application
Select the
BSP location, type a
Project name and click
Finish
The brand new
NIOS II Application should look like:
The next step is to copy all the relevant source code into the software directory.
AD9371/AD9375 No-OS Software
-
Next copy the files intro the src folder of your newly created project. You can do this with Ctrl+C Ctrl+
V or simple drag and drop
-
-
Unzip the archive and go into src→api folder
Next copy the ad9528 and mykonos folder to the src folder of your project. Do NOT copy the common.c and common.h files provided by the api. For now, use the ones downloaded from github.
Transceiver Evaluation Software
-
Next, generate the profile by using the
MATLAB Profile Generator. The profiles can be used with the
Transceiver Evaluation Software to evaluate system performance.
Further, import the profile into TES, and generate the Mykonos initialization structures which are used by the No-
OS driver (Tools → Create Script → C Script). Follow the
AD9370 Quick Start Guide.pdf from AD9371 Transceiver Evaluation Software\Resources folder.
The script generates headless.c, headless.h, myk.c, myk.h and myk_ad9528init.c files. Add myk.c, myk.h and myk_ad9528init.c to the src folder of your project. Do NOT add headless.c and headless.h, instead use the files provided in github.
Note: The AD9371/AD9375 evaluation board contains an on-board voltage controlled crystal oscillator (VCXO), there are limitations with the default hardware configuration in the scenario where user desired device frequencies are not related to the on-board 122.88
MHz VCXO by a rational fraction.
Nios II Eclipse should automatically build the projects and the Console window will display the result of the build. If the build is not done automatically select the Project→Build Automatically menu option.
Note: if you get this error:
warning: Unable to reach (null) (at 0x00088608) from the global pointer (at 0x000752b8) because the offset (78672) is out of the allowed range, -32678 to 32767, a quick workaround can be found on the
Altera support page: modify the linker.x file from your bsp by deleting
+ SIZEOF (.rwdata) from this one line:
At this point the software project setup is complete, the FPGA can be programmed and the software can be downloaded into the system. You can program the FPGA by using
Quartus Prime Programmer. Load your
.sof file and click
Start, the
Progress bar should indicate
100% (Successful)
Next, go to Nios II eclipse and select
Run → Run Configurations…
Select the
Nios II Hardware configuration type.
Press the New button to create a new configuration.
On the
Target Connection tab, press the
Refresh Connections button. You may need to expand the window or scroll to the right to see this button.
Check the Ignore mismatched system ID option.
Check the Ignore mismatched system timestamp option.
Press the Run button in the Run Configurations window.
This will re-build the software project to create an up–to-date executable and then download the code into memory.
Push data into/out of the AD9371/AD9375
Below is defined the dac_core structures used by the dac_setup() and dac_write_custom_data() functions:
typedef struct
{
uint32_t base_address;
uint8_t resolution;
dac_channel *channels;
uint32_t dac_ddr_baseaddr;
}dac_core;
typedef struct
{
uint32_t dds_frequency_tone0; // in hz (1000*1000 for MHz);
uint32_t dds_phase_tone0; // in milli(?) angles (90*1000 for 90 degrees = pi/2)
int32_t dds_scale_tone0; // in micro units (1.0*1000*1000 is 1.0)
uint32_t dds_frequency_tone1; // in hz (1000*1000 for MHz)
uint32_t dds_phase_tone1; // in milli(?) angles (90*1000 for 90 degrees = pi/2)
int32_t dds_scale_tone1; // in micro units (1.0*1000*1000 is 1.0)
uint32_t dds_dual_tone; // if using single tone for this channel, set to 0x0
uint32_t pat_data; // if using SED/debug that sort of thing
dac_data_src sel; // set to one of the enumerated type above.
}dac_channel;
Below is defined the adc_core structure used by the adc_setup() and adc_capture() functions:
typedef struct
{
uint32_t base_address;
uint8_t master;
uint8_t no_of_channels;
uint8_t resolution;
uint32_t start_address;
}adc_core;
DDS Mode
DMA Mode
Set dac_data_src to
DAC_SRC_DMA.
dac_write_custom_data() function takes as argument the sine_lut_iq array which contains the custom data to be transmitted.
The format for each I and Q is 16-bit signed two's complement. I and Q together make up one 32-bit tx sample.
Capture data
Once DDS or
DMA mode is selected and the project configuration can be ran.
Open an
UART terminal, set the baud rate to 115200bps and make sure the initialization was completed, as in the screenshot bellow:
-
By running capture.bat, the iq_rx1.csv and iq_rx2.csv files will be generated inside the nios2eds folder
Start
VisualAnalog and open the
visual_analog.vac file downloaded from the git repository.
From the Pattern Loader window, browse for the newly generated .csv files and click Run.
Download no-OS
The source code of the no-OS software and the scripts can be downloaded from the Analog Devices github.