Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
resources:eval:user-guides:max32670-lr-ardz [21 Mar 2024 03:33] – Replaced photo in Hardware setup section Joyce Velascoresources:eval:user-guides:max32670-lr-ardz [02 Apr 2024 10:41] – [Equipment Needed] Joyce Velasco
Line 408: Line 408:
   * One (1) [[adi>EV-CATTLETAG-ARDZ]] Sensor Node   * One (1) [[adi>EV-CATTLETAG-ARDZ]] Sensor Node
    * One (1) MAX32625PICO Rapid Development Platform with 10-pin ribbon cable    * One (1) MAX32625PICO Rapid Development Platform with 10-pin ribbon cable
-      * with firmware image: {{:resources:eval:user-guides:pa_array:max32625_max32666fthr_if_crc_swd_v1.0.5.bin.zip | MAX32625PICO Firmware}} +      * with firmware image: [[repo>max32625pico-firmware-images/raw/master/bin/max32625_max32670evkit_if_crc_swd_v1.0.3.bin| MAX32625PICO Firmware Image for MAX32670]]
   * One (1) CR123A Battery or any equivalent external DC power supply (+3 V to +4.7 V)   * One (1) CR123A Battery or any equivalent external DC power supply (+3 V to +4.7 V)
      *** Note that this is not included in the kit**      *** Note that this is not included in the kit**
Line 426: Line 426:
 ** **
 <hidden **How to flash the firmware image in the MAX32625PICO** > <hidden **How to flash the firmware image in the MAX32625PICO** >
-  -   Download the firmware image: {{:resources:eval:user-guides:pa_array:max32625_max32666fthr_if_crc_swd_v1.0.5.bin.zip | MAX32625PICO Firmware}}+  -   Download the firmware image: [[repo>max32625pico-firmware-images/raw/master/bin/max32625_max32670evkit_if_crc_swd_v1.0.3.bin| MAX32625PICO Firmware Image for MAX32670]]
   -   Do not connect the MAX32625PICO to the [[adi>MAX32670-LR-ARDZ]] Base Board yet.   -   Do not connect the MAX32625PICO to the [[adi>MAX32670-LR-ARDZ]] Base Board yet.
   -   Connect the MAX32625PICO to the Host PC using the micro USB to USB cable.   -   Connect the MAX32625PICO to the Host PC using the micro USB to USB cable.
resources/eval/user-guides/max32670-lr-ardz.txt · Last modified: 24 Apr 2024 03:43 by erbe reyta