This LoRa Reference Design Base Board consists of the MAX32670 high-reliability, ultralow power microcontroller based on Arm Cortex-M4 processor, and the LR1110 LoRa RF transceiver module.
In order to use this base board, all hardware settings such as the hardware peripheral connections, jumpers and UART switch configurations, power configurations, connectivity options, and the USB connectors and programming connections are provided in this page. Links to the schematics and the layout files are also available below.
The following standard connectors are provided on the base board for customer to use with external add on modules:
Connector Name | Function |
---|---|
DC Power Connector Header | Input range from +4 V to +6 V DC supply voltage |
Battery Holder | Battery holder for CR123A |
Cortex SWD Header | Used for flash programming and debug interface; also, provides a virtual serial port connection to MAX32670 microcontroller |
PMOD_SPI | 12-pin SPI PMOD connector |
PMOD_I2C | 8-pin I2C PMOD connector |
ESP32 Connector | ESP32 Devkit V1 connector |
Arduino Connectors | Arduino Uno Rev3 compatible connectors |
All connector pinouts for the Development Board are described in the table and its schematic diagram below.
These are the wireless connectivity options available to use for Internet of Things (IoT) applications:
These options can be configured by populating C67 with 39 pF for the external antenna or R159 with 0 Ω for on-board RF chip antenna with the center frequency tuned at 915 MHz.
The MAX32670 has a dedicated LoRa chipset on-board from Semtech (LR1110). This chipset comes complete with the full LoRaWan software protocol and stack, allowing the MAX32670 to operate, occupying a small portion of its memory space for the LoRaWan protocol.
The MAX32670 communicates to the LR1110 using the SPI bus, so the users will need to send LoRa commands and data over SPI bus. Library functions calls have been specifically designed to be used with the MAX32670 and LR1110 using SPI bus.
The pins that connect the MAX32670 and the LR1110 are as follows:
There are two (2) ways of powering the eval board, and a user may use any combination of power sources.
Each of the different power modes, provides a different level of control and flexibility. You can find a matrix table of the different power modes and their general function here:
Power Source | Voltage Rails Provided | Peripherals Powered | Function |
---|---|---|---|
Terminal Block (P11) | 3 V to 6 V | - MAX32670 - SPI and I2C PMODs - ESP32 connectors - Arduino connectors - LoRa chip | able to supply ALL voltages any peripheral might need |
Battery Power (BT1) | 3 V and 6 V | - MAX32670 - SPI and I2C PMODs - ESP32 connectors - Arduino connectors - LoRa chip | able to supply ALL voltages any peripheral might need |
The base board provides three buttons for use: S1, S2, and S3.
Button | Function |
---|---|
S1 | can be used to record timestamps and/or assert an interrupt on a falling/rising edge of the DIN signal on MAX31334, an ultralow power RTC with integrated power switch. Initially short to ground via 0-ohm resistor(R4). See the MAX31334 page for more details. |
S2 | provides a hardware RESET to MAX32670 microcontroller. |
S3 | provides a hardware RESET to MAX77675, buck/buck and boost/boost regulators. The manual reset function is useful for forcing a power-down in case communication with the processor fails. |
The base board has five LEDs: DS1, DS2DS3, DS4, and DS5.
Button | Function |
---|---|
DS1 | used as a LED indicator to one of the GPIO of the MAX32670, P0.28. |
DS2 | used as a LED indicator to one of the GPIO of the MAX32670, P0.29. |
DS3 | used as a LED indicator for the voltage output from the power supply. |
DS4 | used as a LED indicator for the voltage output from the MAX31334. |
DS5 | used as a LED indicator for the 3.3 V voltage output from the MAX3130. |
This board uses SWD Interface and uses MAX32625PICO board for programming the on-board MCUs. See the MAX32625PICO page for more details.
The connector used are based off the 10-pin ARM Cortex standard pinout (0.05“ pin spacing). That pinout is common to both JTAG and SWD debug modes and is depicted in the following image.
The debugger board will need to be plugged in via the USB port in order to program any board.
In order to program the MAX32670 node board, that board must be powered by (1) CR123A battery or by an external power supply through P11. Otherwise, there will be no connection between the two boards.
Design and Integration Files