Wiki

This version (12 Oct 2023 09:53) was approved by erbe reyta.The Previously approved version (11 Oct 2023 08:57) is available.Diff

Hardware

The sub-pages listed below contains all hardware-related information about the LoRa Reference Design base board and the various hardware add-on modules that can be used with it.

Each sub-section contains a general description of the board, detailed description of the connectors, jumpers, and buttons (if any). It also provides links to the design support files (schematics, bill of materials, design projects, and technical documentation), as well as internal links to the example demo software projects.

The following boards are currently available:



Navigation - ADI LoRa
Prev.: Main Page

resources/eval/user-guides/lora-reference-design/hardware.txt · Last modified: 12 Oct 2023 09:53 by erbe reyta