Wiki

This version (12 Oct 2023 09:54) was approved by erbe reyta.The Previously approved version (11 Oct 2023 08:19) is available.Diff

LoRa Reference Design User Guide

Introduction

The LoRa reference design is an Arduino-like development platform based on the MAX32670 ultralow power microcontroller (MCU) with integrated power management for processing, control, and connectivity. The MCU system is based on the ARM Cortex-M4 processor, a collection of digital peripherals, embedded SRAM and flash memory, and an analog subsystem which provides clocking, reset, and power management capability. The MAX32670 features industry leading ultralow power, which makes it ideal for Internet of Things (IoT) applications.

The platform comes in an Arduino Uno form factor, with two PMOD connectors, and an ESP32 Dev Kit connector for easy-to-connect sensors and signal conditioning add-on modules. The on-board LoRa connectivity makes this board IoT-ready right out of the box. The solution is complete with working software and hardware, as well as software examples.

The base platform is accompanied with various Analog Devices add-on hardware, but is also compatible with 3rd party hardware. A free programming and debugging tool called Maxim SDK is also provided by Analog Devices.

This User Guide is structured as follows:

  • Tools and Drivers Installation - provides all the necessary steps to download/install/use the MaximSDK tool, along with a quickstart guide to understanding the tools.
  • Gateway Set-up - provides information on how to set up the gateway using Raspberry Pi 4 as the hardware, and ChirpStack v4 for a gateway OS.
  • Hardware Setup - contains hardware-related information about the base board and the various add-on hardware.
  • Example Projects with Setup Instructions - contains detailed descriptions of the software reference designs available for the base board and add-on hardware.
  • Help and Support - provides information on where to get support for any questions regarding the hardware, software, and tools.
resources/eval/user-guides/lora-reference-design.txt · Last modified: 12 Oct 2023 09:54 by erbe reyta