Wiki

The most recent version of this page is a draft.DiffThis version (29 Jun 2023 16:35) was approved by Andrei Grozav.

This is an old revision of the document!


Jupiter SDR HDL Reference Design

This design allows controlling, receiving and transmitting sample stream from/to an ADRV9002 device through two independent source synchronous interface. At the moment, only LVDS interface is supported.

The design supports SDR or DDR modes, one or two lane mode. This is runtime selectable. The complete list of supported adrv9001 modes, can be consulted in the AXI_ADRV9001/AXI_ADRV9002 Interface Core documentation.

Block design

The design has two receive paths and two transmit paths. One of the receive paths (Rx12) has four channels and the other (Rx2) two channels. These can work independently having each two active channels, or just the Rx12 path having four active channels, while Rx2 is disabled. The same applies to the transmit path but in the other direction.

When only the Rx12 path is active with four channels mode the core will take ownership of both source synchronous interfaces. The requirement in this case is that both interfaces run at the same rate.

DAC Interface

  • Has DDS
  • Has PRBS generation

ADC Interface

  • Has PN checking
  • Has data formater
  • Has programmable input delay

SW programming

Register map

Address IP
0x44A00000 axi_adrv9001
0x44A30000 axi_adrv9001_rx1_dma
0x44A40000 axi_adrv9001_rx2_dma
0x44A50000 axi_adrv9001_tx1_dma
0x44A60000 axi_adrv9001_tx2_dma
0x44A70000 pl_sysmon
0x45000000 axi_sysid_0

SPI connections

SPI manager instance Alias SPI address SPI subordinate CSn
psu spi 0 spi_fpga 0xFF040000 ADRV9002 0

PL Interrupts

Instance HDL interrupt Linux PsU interrupt
0 89
1 90
2 91
3 92
4 93
5 94
6 95
7 96
axi_spi_adl5960_1 8 104
axi_spi_busf 9 105
axi_adrv9002_tx2_dma 10 106
axi_adrv9002_tx1_dma 11 107
axi_adrv9002_rx2_dma 12 108
axi_adrv9002_rx1_dma 13 109
14 110
15 111

ZYNQ U PS EMIO GPIO signals translation from schematic to GPIO number

Ps8 EMIO offset = 78

HW Signal HDL Signal PS GPIO HDL GPIO EMIOn Direction
IO_L7N_66_FAN_CTL fan_ctl 145 67 O
IO_66_USB_FLASH_PROG_EN usb_flash_prog_en 144 66 O
IO_L4N_64_ADRV9002_MCSSRC adrv9002_mcssrc 143 65 O
-- (internal) mcs_or_system_sync_n 142 64 O
IO_L1P_T0L_N0_DBC_64 add_on_power 141 63 O
IO_L23N_T3U_N9_64 add_on_gpio[14] 140 62 I/O
IO_L23P_T3U_N8_64 add_on_gpio[13] 139 61 I/O
IO_L21N_T3L_N5_AD8N_64 add_on_gpio[12] 138 60 I/O
IO_L21P_T3L_N4_AD8P_64 add_on_gpio[11] 137 59 I/O
IO_L2N_T0L_N3_64 add_on_gpio[10] 136 58 I/O
IO_L2P_T0L_N2_64 add_on_gpio[ 9] 135 57 I/O
IO_L1N_T0L_N1_DBC_64 add_on_gpio[ 8] 134 56 I/O
IO_L12N_AD0N_26 add_on_gpio[ 7] 133 55 I/O
IO_L12P_AD0P_26 add_on_gpio[ 6] 132 54 I/O
IO_L11N_AD1N_26 add_on_gpio[ 5] 131 53 I/O
IO_L11P_AD1P_26 add_on_gpio[ 4] 130 52 I/O
IO_L10N_AD2N_26 add_on_gpio[ 3] 129 51 I/O
IO_L10P_AD2P_26 add_on_gpio[ 2] 128 50 I/O
IO_L9N_AD3N_26 add_on_gpio[ 1] 127 49 I/O
IO_L9P_AD3P_26 add_on_gpio[ 0] 126 48 I/O
-- (internal) gpio_rx1_enable_in 126 47 I/O
-- (internal) gpio_rx2_enable_in 126 46 I/O
-- (internal) gpio_tx1_enable_in 126 45 I/O
-- (internal) gpio_tx2_enable_in 126 44 I/O
IO_L18P_64_ADRV9002_DGPIO_11 dgpio[11] 121 43 I/O
IO_L18N_64_ADRV9002_DGPIO_10 dgpio[10] 120 42 I/O
IO_L9N_64_ADRV9002_DGPIO_9 dgpio[ 9] 119 41 I/O
IO_L9P_64_ADRV9002_DGPIO_8 dgpio[ 8] 118 40 I/O
IO_T2U_N12_64_ADRV9002_DGPIO_7 dgpio[ 7] 117 39 I/O
IO_L14N_64_ADRV9002_DGPIO_6 dgpio[ 6] 116 38 I/O
IO_L7N_64_ADRV9002_DGPIO_5 dgpio[ 5] 115 37 I/O
IO_L7P_64_ADRV9002_DGPIO_4 dgpio[ 4] 114 36 I/O
IO_L6N_64_ADRV9002_DGPIO_3 dgpio[ 3] 113 35 I/O
IO_L6P_64_ADRV9002_DGPIO_2 dgpio[ 2] 112 34 I/O
IO_L5N_64_ADRV9002_DGPIO_1 dgpio[ 1] 111 33 I/O
IO_L5P_64_ADRV9002_DGPIO_0 dgpio[ 0] 110 32 I/O
IO_L8N_AD4N_26 ext_gpio[15] 109 31 I/O
IO_L8P_AD4P_26 ext_gpio[14] 108 30 I/O
IO_L7N_AD5N_26 ext_gpio[13] 107 29 I/O
IO_L7P_AD5P_26 ext_gpio[12] 106 28 I/O
IO_L6N_AD6N_26 ext_gpio[11] 105 27 I/O
IO_L6P_AD6P_26 ext_gpio[10] 104 26 I/O
IO_L5N_AD7N_26 ext_gpio[ 9] 103 25 I/O
IO_L5P_AD7P_26 ext_gpio[ 8] 102 24 I/O
IO_L4N_AD8N_26 ext_gpio[ 7] 101 23 I/O
IO_L4P_AD8P_26 ext_gpio[ 6] 100 22 I/O
IO_L3N_AD9N_26 ext_gpio[ 5] 99 21 I/O
IO_L3P_AD9P_26 ext_gpio[ 4] 98 20 I/O
IO_L2N_AD10N_26 ext_gpio[ 3] 97 19 I/O
IO_L2P_AD10P_26 ext_gpio[ 2] 96 18 I/O
IO_L1N_AD11N_26 ext_gpio[ 1] 95 17 I/O
IO_L1P_AD11P_26 ext_gpio[ 0] 94 16 I/O
IO_L17N_RF_TX2_MUX_CTL2 rf_tx2_mux_ctl2 93 15 O
IO_L17P_RF_TX2_MUX_CTL1 rf_tx2_mux_ctl1 92 14 O
IO_L16N_RF_TX1_MUX_CTL2 rf_tx1_mux_ctl2 91 13 O
IO_L16P_RF_TX1_MUX_CTL1 rf_tx1_mux_ctl1 90 12 O
IO_L13P_RF_RX2B_MUX_CTL rf_rx2b_mux_ctl 89 11 O
IO_L14P_RF_RX2A_MUX_CTL rf_rx2a_mux_ctl 88 10 O
IO_L15P_RF_RX1B_MUX_CTL rf_rx1b_mux_ctl 87 9 O
IO_L15N_RF_RX1A_MUX_CTL rf_rx1a_mux_ctl 86 8 O
-- (internal) mssi_sync 85 7 O
VIN_POE_VALID_N vin_poe_valid_n 84 6 I
VIN_USB2_VALID_N vin_usb2_valid_n 83 5 I
VIN_USB1_VALID_N vin_usb1_valid_n 82 4 I
IO_66_ADRV9002_CLKSRC clksrc 81 3 O
IO_65_ADRV9002_MODE mode 80 2 O
IO_65_ADRV9002_RST resetb 79 1 O
IO_L24P_65_ADRV9002_GP_INT gp_int 78 0 I

Source code

Building the HDL project

To build the project follow the build documentation.

More Information

Support

Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.

/srv/wiki.analog.com/data/pages/resources/eval/user-guides/jupiter_sdr/reference_hdl.txt · Last modified: 15 Sep 2023 13:20 by Andrei Grozav