This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:inertial-mems:imu:imu-evaluation-software [17 Feb 2021 05:06] – Fixed English Juan Chong | resources:eval:user-guides:inertial-mems:imu:imu-evaluation-software [17 Feb 2021 05:13] (current) – Fixed English Juan Chong | ||
---|---|---|---|
Line 36: | Line 36: | ||
- The **Devices** menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the [[adi> | - The **Devices** menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the [[adi> | ||
- | - The **Register Access** option calls a sub-menu that lists all user-configurable registers available from the part number selected in the " | + | - The **Register Access** option calls a sub-menu that lists all user-configurable registers available from the part number selected in the " |
- The **Data Capture** option calls a sub-menu designed to enable synchronous data logging from the selected device. | - The **Data Capture** option calls a sub-menu designed to enable synchronous data logging from the selected device. | ||
Line 48: | Line 48: | ||
The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the **Read** button (identified by a red box). | The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the **Read** button (identified by a red box). | ||
- | The yellow box shows three waveform recorder windows. Each window allows for plotting the three, primary sensor types (gyroscopes, | + | The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, |
==== Register Access ==== | ==== Register Access ==== | ||
Line 108: | Line 108: | ||
- **Add File Header** - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file | - **Add File Header** - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file | ||
- | - **Use Scaled Data** - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement), scaled number. For example, when this option is enabled, be in units of degrees/ | + | - **Use Scaled Data** - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/ |
===== Software Revision History ===== | ===== Software Revision History ===== | ||
Line 126: | Line 126: | ||
|v1.9.7 | 8/21/2013| Corrected scale factors associated with GYRO_OUT/ | |v1.9.7 | 8/21/2013| Corrected scale factors associated with GYRO_OUT/ | ||
|v1.9.6 | N/A| Extended Precision Auto Null Wait time to 30 seconds on ADIS1636x/ | |v1.9.6 | N/A| Extended Precision Auto Null Wait time to 30 seconds on ADIS1636x/ | ||
- | | | | NOTE: This version was not posted online but these updates are in current versions | | + | | | | NOTE: This version was not posted online, but these updates are in current versions | |
|v1.9.5 | N/A | Corrected scale factors and offset factors associated with xTEMP_OUT on the ADIS16445 | | |v1.9.5 | N/A | Corrected scale factors and offset factors associated with xTEMP_OUT on the ADIS16445 | | ||
| | | Corrected scale factors and offset factors associated with xTEMP_OUT and xMAGN_OUT registers in the ADIS16448| | | | | Corrected scale factors and offset factors associated with xTEMP_OUT and xMAGN_OUT registers in the ADIS16448| | ||
- | | | | NOTE: This version was not posted online but these updates are in current versions | | + | | | | NOTE: This version was not posted online, but these updates are in current versions | |
|v1.9.4 | N/A | Enabled support for using an external clock on the ADIS16405| | |v1.9.4 | N/A | Enabled support for using an external clock on the ADIS16405| | ||
- | | | | NOTE: This version was not posted online but these updates are in current versions | | + | | | | NOTE: This version was not posted online, but these updates are in current versions | |
|v1.9.3 | 3/18/2013| Added support for the ADIS16400 and ADIS16405| | |v1.9.3 | 3/18/2013| Added support for the ADIS16400 and ADIS16405| | ||
|v1.9.2 | 2/18/2013| Changed the separation " | |v1.9.2 | 2/18/2013| Changed the separation " | ||
Line 141: | Line 141: | ||
|v1.7.0 | 10/1/12 | Added support for the ADIS16360, ADIS16362, ADIS16364, ADIS16365, and ADIS16367 | | |v1.7.0 | 10/1/12 | Added support for the ADIS16360, ADIS16362, ADIS16364, ADIS16365, and ADIS16367 | | ||
| | | Corrected a scaling issue for those who use " | | | | Corrected a scaling issue for those who use " | ||
- | | | | NOTE: Some sensitivity was still observed; some users in Turkey may need to change regional setting to fully address. | | + | | | | NOTE: Some sensitivity was still observed; some users in Turkey may need to change |
|v1.6.0 | 9/3/12 | Added support for the ADIS16300 and ADIS16305 | | |v1.6.0 | 9/3/12 | Added support for the ADIS16300 and ADIS16305 | | ||
|v1.5.0 |8/22/12 | Added support for the ADIS16445 | | |v1.5.0 |8/22/12 | Added support for the ADIS16445 | | ||
|v1.4.0 |7/18/12 | Added support for the ADIS1613, ADIS16135, ADIS16136 and ADIS16334 | | |v1.4.0 |7/18/12 | Added support for the ADIS1613, ADIS16135, ADIS16136 and ADIS16334 | | ||
|v1.3.0 | N/A | Internal updates | | |v1.3.0 | N/A | Internal updates | | ||
- | | | | NOTE: This version was not posted online but these updates are in current versions | | + | | | | NOTE: This version was not posted online, but these updates are in current versions | |
|v1.2.0 | 5/28/2012| Added support for the ADIS16480| | |v1.2.0 | 5/28/2012| Added support for the ADIS16480| | ||
| | | Added 3-D viewer for ADIS16480 demonstration| | | | | Added 3-D viewer for ADIS16480 demonstration| |