Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [01 Dec 2017 16:39] – [SETUP WITH ADIS1633X/44X IMUS] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [19 Oct 2023 17:52] (current) – [GENERAL DESCRIPTION] Mark Looney |
---|
====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== | ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== |
=====GENERAL DESCRIPTION===== | =====GENERAL DESCRIPTION===== |
The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the EVAL-ADIS2 evaluation system. | The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] or EVAL-ADIS2 (obsolete) evaluation systems. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_adis1644x_flex_02.png?500|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_adis1644x_flex_02.png?500|}} |
| |
<WRAP alert>**WARNING!** The connector pin numbers on the ADIS1644X/FLEX do not match those on the ADIS1633x and ADIS1644x IMUs</WRAP> | |
| |
The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with: | The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with: |