Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [01 Dec 2017 20:54] – old revision restored (12 May 2017 20:52) Mark Looneyresources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [19 Oct 2023 17:52] (current) – [GENERAL DESCRIPTION] Mark Looney
Line 1: Line 1:
 ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ======
 =====GENERAL DESCRIPTION===== =====GENERAL DESCRIPTION=====
-The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]].  This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the EVAL-ADIS2 evaluation system.+The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]].  This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] or EVAL-ADIS2 (obsolete) evaluation systems.
    
 {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}}
resources/eval/user-guides/inertial-mems/imu/adis16imu2-pcb.txt · Last modified: 19 Oct 2023 17:52 by Mark Looney