This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [23 Dec 2016 22:50] – [SETUP WITH ADIS1636x/40X IMUs] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [01 Dec 2017 20:54] – old revision restored (12 May 2017 20:52) Mark Looney | ||
---|---|---|---|
Line 51: | Line 51: | ||
For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi> | For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi> | ||
+ | =====KEY PHYSICAL DIMENSIONS===== | ||
+ | Please see the following diagram for dimensions of all key physical attributes: | ||
+ | |||
+ | {{: | ||
+ | |||
+ | |||
=====INTERFACE CONNECTOR===== | =====INTERFACE CONNECTOR===== | ||
J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. |