This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb [05 Aug 2017 19:51] – [ADIS16375, ADIS16480, ADIS16485, ADIS16488 Mounting] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb [31 Aug 2017 15:57] – [ADIS16490 Mounting] Mark Looney | ||
---|---|---|---|
Line 58: | Line 58: | ||
{{: | {{: | ||
- | ===JP1 Connection=== | + | ==== ADIS16490, ADIS16495, ADIS16497 |
- | + | ||
- | When evaluating the ADIS16375 or any of the ADIS1648x family of IMUs, make sure that JP1 is installed. | + | |
- | + | ||
- | ==== ADIS16490 | + | |
=== STEP #1 === | === STEP #1 === | ||
Line 104: | Line 100: | ||
{{: | {{: | ||
- | =====Connecting | + | =====JP1 Settings===== |
+ | |||
+ | Please use the following table to determine how to use JP1 on the ADIS16IMU1/ | ||
+ | |||
+ | ^ DUT MODEL NUMBER^ JP1 INSTALLED? ^ | ||
+ | |ADIS16133 | NO | | ||
+ | |ADIS16135 | NO | | ||
+ | |ADIS16136 | NO | | ||
+ | |ADIS16137 | NO | | ||
+ | |ADIS16360 | NO | | ||
+ | |ADIS16362 | NO | | ||
+ | |ADIS16364 | NO | | ||
+ | |ADIS16365 | NO | | ||
+ | |ADIS16367 | NO | | ||
+ | |ADIS16400 | NO | | ||
+ | |ADIS16405 | NO | | ||
+ | |ADIS16407 | NO | | ||
+ | |ADIS16375 | YES | | ||
+ | |ADIS16480 | YES | | ||
+ | |ADIS16485 | YES | | ||
+ | |ADIS16488 | YES | | ||
+ | |ADIS16488A | YES | | ||
+ | |ADIS16490 | NO | | ||
+ | |ADIS16495 | NO | | ||
+ | |ADIS16497 | NO | | ||
+ | |||
+ | =====CONNECTING TO THE EVAL-ADIS2===== | ||
This can also connect to J1 on the EVAL-ADIS2 | This can also connect to J1 on the EVAL-ADIS2 | ||