This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb [21 Aug 2019 03:19] – [Ribbon Cable Options] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb [21 Aug 2019 03:32] – [INTERFACE CONNECTOR] Mark Looney | ||
---|---|---|---|
Line 104: | Line 104: | ||
=====JP1 Settings===== | =====JP1 Settings===== | ||
- | JP1 controls the ???. | + | JP1 controls the power supply to teh VDDRTC function, on the ADIS16375, ADIS16480, ADIS16485 and ADIS16488A products. For all other products, do not install JP1. |
+ | |||
Please use the following table to determine how to use JP1 on the ADIS16IMU1/ | Please use the following table to determine how to use JP1 on the ADIS16IMU1/ | ||
Line 138: | Line 139: | ||
===== INTERFACE CONNECTOR ===== | ===== INTERFACE CONNECTOR ===== | ||
- | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector | + | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector. |
==== Pin Assignments ===== | ==== Pin Assignments ===== | ||
Line 147: | Line 147: | ||
==== Ribbon Cable Options ==== | ==== Ribbon Cable Options ==== | ||
- | Check out the [[https:// | + | Check out the [[https:// |