The ADIS16COM1/PCBZ provides a breakout function for the ADIS16000CMLZ, which pairs with the ADIS16229AMLZ to provide the sensor, signal processing and transceiver function for a wireless vibration sensing system.
Here is a picture of the contents that come with the ADIS16COM1/PCBZ.
The ADIS16COM1/PCBZ provides 4 mounting holes that line up with mounting “A” Labeled holes on the EVAL-ADIS and supports the following products: ADIS16000AMLZ ADIS16229AMLZ products. Please see the following picture for device mounting hole locations.
Use the M2x0.4x6mm machine screws (provided in pink bag ANALOGKIT2) for mounting the ADIS16COM1/PCBZ to the EVAL-ADIS and set their torque for 20 inch-ounces. The red-highlights in the top-view picture illustrate the location of the mounting holes.
Use the M3x0.5x12mm machine screws and M3x.5x Hex nuts with the M3 washers optional(provided in pink bag ANALOGKIT2) for mounting ADIS16000AMLZ product to the ADIS16COM1/PCBZ and set their torque for 20 inch-ounces. The red-highlights in the top-view picture illustrate the location of the mounting holes for these products. Attach the 16 pin ribbon cable included with the EVAL-ADIS to connect the J1 connectors. For high-vibration environments, consider using more than 2 screws, per AN-1045
WARNING: Make sure that the connector pins are in alignment with J1 on the EVAL-ADIS and J1 on the ADIS16COM1/PCBZ, before pressing it into place.
Here is a close-up view, which shows a few slides of the correct connector alignment .