Wiki

This version (14 Jan 2021 05:34) was approved by Robin Getz.The Previously approved version (10 Apr 2019 17:27) is available.Diff

ADIS1650x-x/PCBZ QUICK START EVALUATION WIKI GUIDE

1. Follow Steps 2 through 4 of the EVAL-ADIS2 Evaluation System Wiki. These step contain detailed instructions on connecting the hardware and installing the SDP drivers. EVAL-ADIS2 Evaluation System (note that the ADIS1505x will not be listed in the list of supported devices because it's not released.

2. Download the latest ADIS evaluation software from ADI FTP site. (Note that this is a standalone .EXE file that can reside anywhere on the user's PC.)

3.

The Evaluation Software Interface

The Device Menu allows the user to

Using the Data Logging Function

resources/eval/user-guides/inertial-mems/imu/adis1650x_quick_start_evaluation_wiki_guide.txt · Last modified: 14 Jan 2021 05:24 by Robin Getz