Wiki

This version is outdated by a newer approved version.DiffThis version (03 Jan 2021 22:08) was approved by Robin Getz.The Previously approved version (12 Nov 2019 19:31) is available.Diff

This is an old revision of the document!


ADIS1650x-x/PCBZ BREAKOUT BOARD WIKI GUIDE

OVERVIEW

There are seven (7) breakout boards that support ADIS1650x IMU products. These breakout boards that provide a simple way to develop a prototype connection between the ADIS1650x IMUs and an existing embedded processor platform. This breakout board already contains the ADIS1650x IMU and one 16-pin header, which mates to 2 mm ribbon cables. As a general guideline, these breakout boards will support reliable communications over ribbon cables that are up to 20 cm in length, but it is always a good idea to validate signal integrity before relying on this type of connection to support a critical communication link.

PART NUMBER SUMMARY

Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board.

MODEL NUMBERS MEASUREMENT RANGE
BREAKOUT BOARD IMU GYROSCOPE ACCELEROMETER
ADIS16500/PCBZ ADIS16500AMLZ +/-2000 dps +/-40g
ADIS16505-1/PCBZ ADIS16505-1BMLZ +/-125 dps +/-8g
ADIS16505-2/PCBZ ADIS16505-2BMLZ +/-500 dps +/-8g
ADIS16505-3/PCBZ ADIS16505-3BMLZ +/-2000 dps +/-8g
ADIS16507-1/PCBZ ADIS16507-1BMLZ +/-125 dps +/-40g
ADIS16507-2/PCBZ ADIS16507-2BMLZ +/-500 dps +/-40g
ADIS16507-3/PCBZ ADIS16507-3BMLZ +/-2000 dps +/-40g

The primary attributes that differentiate each of these models are measurement range (gyroscopes and accelerometers) and the calibration temperature range.

EVAL-ADIS2 CONNECTION

The J1 connector on each ADIS1650x-x/PCBZ breakout board is pin-for-pin compatible with the same connector (J1) on the EVAL-ADIS2 evaluation system. The picture below shows the EVAL-ADIS2 connectors.

If connecting an external power supply, refer to the picture below for the polarity of the J3 external power connector:

The user should follow these steps when connecting the xxx to the EVAL-ADIS2 evaluation system:

1. Ensure that Jumper JP1 is straddling the left “+3.3V REG” pin and the center pin, assuming the EVAL-ADIS2 board is oriented with the Mini-USB connector is on the left-hand side.

Note: If the user wishes to use an external power supply, move the JP1 jumper so that it straddles the center and lower pin and connect the external supply to Connector J3. GND is the left pin and VDD (+3.3 V) is the right pin.

2. Connect the ribbon cable between the EVAL-ADIS2 and ADIS1650x-x evaluation board.

3. Install the SDP Drivers from EVAL-ADIS2 USB Drivers.

3. Install the ADIS-EVAL2 Evaluation software from EVAL-ADIS2 Evaluation Software

4. Connect the EVAL-ADIS2 USB cable to the PC and verify that LED1 and LED2 are illuminated on the EVAL-ADIS2 board.

5. More information regarding the EVAL-ADIS2 evaluation system can be found at: EVAL-ADIS2 Wiki Guide

6. More information regarding the operation of the evaluation software can be found at: adis1650x_evalguide_pr.c.pdf

DIMENSTIONS/MOUNTING HOLES

These breakout boards have four mounting holes (one in each corner) which support attachment to another surface with M2 machine screws. Please see the following diagram for more details:

INTERFACE CONNECTOR

Please see the following table for the pin assignments for the interface connector (J1)

PIN NAME DESCRIPTION
1 ~RST Reset, Active Low
2 SCLK Serial Clock (Serial Peripheral Interface)
3 ~CS Chip Select (Serial Peripheral Interface), Active Low
4 DOUT Data Output (Serial Peripheral Interface)
5 DNC Do not connect
6 DIN Data Input (Serial Peripheral Interface)
7 GND Ground
8 GND Ground
9 GND Ground
10 VDD Power Supply, +3.3V
11 VDD Power Supply, +3.3V
12 VDD Power Supply, +3.3V
13 DR Data Ready
14 SYNC Sync Input
15 DNC Do not connect
16 DNC Do not connect

CABLING

J1 supports connection with the following style of cables: 2.00 mm IDC Ribbon Cable Assembly

TIP: Use “2.00 mm IDC Ribbon Cable Assembly” as search criteria to find the latest options on the market.

At the time of initial release for these breakout boards, we were most familiar with the TCSD Series from Samtec.

ELECTRICAL SCHEMATIC

The following diagram illustrates the electrical schematic for the ADIS16500/PCBZ. Please note that the only difference in the other models will be in the IMU (ADIS16470AMLZ is shown in the following view). Click on this image to access a higher-resolution view.

REFERENCE DESIGNS & CODE EXAMPLES

This section provides a list of reference designs for those who are ready to evaluate the ADIS1650x. These references designs include one or both of the following:

- The physical connection between the ADIS1647x-x/PCB and a specific embedded processor platform/system

- Embedded code that lists all ADIS1650x user registers, manages the ADIS1650x's SPI protocol requirements, and provides examples for accessing the ADIS1650x's registers

ADI IMU Linux drivers

resources/eval/user-guides/inertial-mems/imu/adis1650x-pcb.1609707856.txt.gz · Last modified: 03 Jan 2021 22:04 by Robin Getz