Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:imu:adis1649x [01 Nov 2016 19:20]
Mark Looney [EVAL-ADIS USB Driver Installation]
resources:eval:user-guides:inertial-mems:imu:adis1649x [22 Feb 2019 22:27]
Paul Kern [EVAL-ADIS USB Driver Installation]
Line 1: Line 1:
 ====== ADIS1649x EVALUATION GUIDE ====== ====== ADIS1649x EVALUATION GUIDE ======
-There are several ​tools that provide support for early evaluation of the IMUs in the ADIS1649x product family. Here is a quick summary of the tools that are available:+The following ​tools that provide support for early evaluation of IMUs in the ADIS1649x product family:
  
   * The [[adi>​EVAL-ADIS16IMU1|ADIS16IMU1/​PCBZ]] is the **__breakout board__** for the ADIS1649x, which provides a simple way to connect to the ADIS1649x using a 16-pin, 1mm ribbon cable. ​   * The [[adi>​EVAL-ADIS16IMU1|ADIS16IMU1/​PCBZ]] is the **__breakout board__** for the ADIS1649x, which provides a simple way to connect to the ADIS1649x using a 16-pin, 1mm ribbon cable. ​
Line 31: Line 31:
  
 ===STEP #1=== ===STEP #1===
-Visit the [[adi>​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL-ADIS2.html#​eb-relatedsoftware|Software]] section of the [[adi>​eval-ads2|EVAL-ADIS2]] web page to download the latest driver file, which is typically an executable file that inside of a zipped file (USB_Installation.zip,​ for example). ​+Visit the [[adi>​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL-ADIS2.html#​eb-relatedsoftware|Software]] section of the [[adi>​eval-adis2|EVAL-ADIS2]] web page to download the latest driver file, which is typically an executable file that inside of a zipped file (USB_Installation.zip,​ for example). ​
  
 ===STEP #2=== ===STEP #2===
resources/eval/user-guides/inertial-mems/imu/adis1649x.txt · Last modified: 22 Feb 2019 22:27 by Paul Kern