Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis1649x [01 Nov 2016 19:16] – [EVAL-ADIS USB Driver Installation] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis1649x [22 Feb 2019 22:27] (current) – [EVAL-ADIS USB Driver Installation] Paul Kern |
---|
====== ADIS1649x EVALUATION GUIDE ====== | ====== ADIS1649x EVALUATION GUIDE ====== |
There are several tools that provide support for early evaluation of the IMUs in the ADIS1649x product family. Here is a quick summary of the tools that are available: | The following tools that provide support for early evaluation of IMUs in the ADIS1649x product family: |
| |
* The [[adi>EVAL-ADIS16IMU1|ADIS16IMU1/PCBZ]] is the **__breakout board__** for the ADIS1649x, which provides a simple way to connect to the ADIS1649x using a 16-pin, 1mm ribbon cable. | * The [[adi>EVAL-ADIS16IMU1|ADIS16IMU1/PCBZ]] is the **__breakout board__** for the ADIS1649x, which provides a simple way to connect to the ADIS1649x using a 16-pin, 1mm ribbon cable. |
| |
===STEP #1=== | ===STEP #1=== |
Visit the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADIS2.html#eb-relatedsoftware|Software]] section of the [[adi>eval-ads2|EVAL-ADIS2]] web page to download the latest driver file, which is typically an executable file that inside of a zipped file (USB_Installation.zip, for example). | Visit the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADIS2.html#eb-relatedsoftware|Software]] section of the [[adi>eval-adis2|EVAL-ADIS2]] web page to download the latest driver file, which is typically an executable file that inside of a zipped file (USB_Installation.zip, for example). |
| |
===STEP #2=== | ===STEP #2=== |
Click on **Next** when this window pops up. | Click on **Next** when this window pops up. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16490_wg_000.png?600|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16490_wg_0000.png?600|}} |
| |
===STEP #5=== | ===STEP #5=== |