Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis1646x [09 Oct 2017 16:46] – [ADIS1646X/AD24000 EVALUATION ON A PC] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis1646x [07 Apr 2023 17:56] (current) – [SETUP] Mark Looney |
---|
| |
===== OVERVIEW ===== | ===== OVERVIEW ===== |
Evaluating the [[adi>ADIS16460|ADIS16460]] and the AD24000 on a PC requires the use of the [[adi>EVAL-ADIS16IMU4|ADIS16IMU4/PCBZ]] and [[adi>EVAL-ADIS|EVAL-ADIS]]. Aside from this section of the datasheet, the instruction text and graphics identify only the ADIS16460. However, all of these instructions apply to the AD24000 in the same manner. Mention of AD24000 is omitted only to simplify the text. | Evaluating the [[adi>ADIS16460|ADIS16460]] and the AD24000 on a PC requires the use of the [[adi>EVAL-ADIS16IMU4|ADIS16IMU4/PCBZ]] and [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]]. Aside from this section of the datasheet, the instruction text and graphics identify only the ADIS16460. However, all of these instructions apply to the AD24000 in the same manner. Mention of AD24000 is omitted only to simplify the text. |
| |
| |
1. Install the DUT (for example, an ADIS16460AMLZ) onto the ADIS16IMU4/PCBZ | 1. Install the DUT (for example, an ADIS16460AMLZ) onto the ADIS16IMU4/PCBZ |
| |
2. Connect the ADIS16IMU4/PCBZ to the EVAL-ADISZ | 2. Connect the ADIS16IMU4/PCBZ to the EVAL-ADIS-FX3Z |
| |
3. Set JP1 Jumper on EVAL-ADISZ | 3. Set JP1 Jumper on EVAL-ADIS-FX3Z |
| |
====ADIS1646x Installation on the ADIS16IMU4/PCBZ==== | ====ADIS1646x Installation on the ADIS16IMU4/PCBZ==== |
| |
==== Gyroscope Demonstration ==== | ==== Gyroscope Demonstration ==== |
[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#gyroscope_demonstration|Click here to see a gyroscope demonstration, from the ADIS16448 Wiki Site]]. | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#gyroscope_demonstration|Click here to see a gyroscope demonstration, from the ADIS16448 Wiki Site]]. |
| |
==== Accelerometer Demonstration, Static ==== | ==== Accelerometer Demonstration, Static ==== |
[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_gravity|Click here to see the static (gravity) accelerometer demonstration, from the ADIS16448 Wiki Site]]. | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_gravity|Click here to see the static (gravity) accelerometer demonstration, from the ADIS16448 Wiki Site]]. |
| |
==== Accelerometer Demonstration, Dynamic ==== | ==== Accelerometer Demonstration, Dynamic ==== |
[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_dynamic|Click here to see the dynamic accelerometer demonstration, from the ADIS16448 Wiki Site]]. | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_dynamic|Click here to see the dynamic accelerometer demonstration, from the ADIS16448 Wiki Site]]. |
| |
==== Useful Experiments ==== | ==== Useful Experiments ==== |
Click on the following links to access several useful experiments in ADI's Engineer Zone/MEMS Community. | Click on the following links to access several useful experiments in ADI's Engineer Zone/MEMS Community. |
| |
[[http://ez.analog.com/docs/DOC-2181|Gyroscope Sensitivity Measurement]] | [[ez>docs/DOC-2181|Gyroscope Sensitivity Measurement]] |
| |
[[http://ez.analog.com/docs/DOC-2212|Gyroscope Noise Density]] | [[ez>docs/DOC-2212|Gyroscope Noise Density]] |
| |
[[http://ez.analog.com/docs/DOC-2162|Gyroscope In-Run Bias Stability]] | [[ez>docs/DOC-2162|Gyroscope In-Run Bias Stability]] |
| |
[[http://ez.analog.com/docs/DOC-2163|Gyroscope Angle Random Walk]] | [[ez>docs/DOC-2163|Gyroscope Angle Random Walk]] |
| |
[[http://ez.analog.com/docs/DOC-2223|ADIS16480 3-D Demonstration]] | [[ez>docs/DOC-2223|ADIS16480 3-D Demonstration]] |
| |
| |