This is an old revision of the document!
Evaluating the ADIS16460 and the AD24000 on a PC requires the use of the ADIS16IMU4/PCBZ and EVAL-ADIS. Aside from this section of the datasheet, the instruction text and graphics identify only the ADIS16460. However, all of these instructions apply to the AD24000 in the same manner. Mention of AD24000 is omitted only to simplify the text.
The physical setup requires only three simple steps:
1. Install the DUT (for example, an ADIS16460AMLZ) onto the ADIS16IMU4/PCBZ
2. Connect the ADIS16IMU4/PCBZ to the EVAL-ADISZ
3. Set JP1 Jumper on EVAL-ADISZ
JUMPER | SETTING |
---|---|
JP1 | +3.3V |
JP2 | Not used, may want to leave it in place for safety reasons |
Click here to download the latest version of the IMU Evaluation software.
Click here to download the latest drivers for the EVAL-ADIS2.
The IMU Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to most ADIS16xxx products. This platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition, which is synchronous with data production of each ADIS16xxx.
Once the IMU Evaluation software loads, you should be presented with a window similar to the image shown below.
The image below has been color-coded to illustrate the different parts of the IMU Evaluation Software. These colored sections will be referred to in the following sections.
The drop-down menus highlighted in orange list additional features and utilities that make up the core functionality of the evaluation software.
- The Devices menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the ADIS16448 is selected.
- The Register Access option calls a sub-menu that lists all user-configurable registers available from the part number selected in the “Devices” drop-down menu. It also provides read/write access to each register.
- The Data Capture option calls a sub-menu designed to enable synchronous data logging from the selected device.
- The Demos option calls a 3-D visualization tool. This feature is only supported for the ADIS16480 and ADIS16448 devices.
- The Tools option calls a sub-menu that displays USB diagnostic information.
- The About option provides more detailed software revision information.
The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the Read button (identified by a red box).
The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, accelerometers, and magnetometers [if supported]). The top subplot displays gyroscope data, the middle plot displays accelerometer data and the bottom plot displays magnetometer data. Each plot color corresponds to the colors displayed in the “Output Registers” window (highlighted in purple).
The Register Access window provides read and write access to all user-accessible registers listed in the selected device's datasheet. The image below shows a screenshot of the window.
The color-coded image below is referenced in the following section.
The purple box sorts each set of registers into a standard category. The available categories are:
- Control/Status - General sensor configuration, alarm, and metadata registers
- Output - Inertial sensor output registers
- Calibration - User offset and misc. calibration registers
The section highlighted by the red box lists all of the registers in the selected category. Click on the register name to select a register for individual read/write access.
The green box identifies the read/write control options for the current register selection.
The Update Registers in Category button (shown in an orange box above) automatically reads all of the registers shown in the selected category (red box) and updates their contents in the GUI.
The section highlighted in yellow identifies provides a means of easily calling subroutines within the connected sensor. Clicking on a button is equivalent to writing a single-bit command to the respective register.
The Save Reg Settings to File programmatically reads and saves the contents of all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads a target .csv file and attempts to write the saved values back into the sensor.
The Data Capture window only supports synchronous data acquisition and logging to a file on the host PC. Data samples are only read from the sensor when the data ready pin toggles, indicating that data is valid.
The color-coded image below is referenced in the following section.
The section highlighted in red lists all of the registers that are eligible for data capture. Checking the box next to each register indicates that the specified register values should be recorded once the data stream begins.
The section highlighted in green allows for customizing the file name and location of the resultant .csv files.
The section highlighted in yellow identifies the data stream configuration options.
- Record Length - The total number of samples to be captured. A sample is defined as a single “data valid” period as signaled by the data ready pin on the sensor
- Sample Rate - The instantaneous data ready rate as measured by the evaluation board
- Capture Time - The estimated data capture time in DD:HH:MM:SS format calculated based upon the instantaneous sample rate
- Add File Header - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file
- Use Scaled Data - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/second
Click here to download the latest version of the IMU Evaluation software.
Click here to download the latest drivers for the EVAL-ADIS2.
The IMU Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to most ADIS16xxx products. This platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition, which is synchronous with data production of each ADIS16xxx.
Once the IMU Evaluation software loads, you should be presented with a window similar to the image shown below.
The image below has been color-coded to illustrate the different parts of the IMU Evaluation Software. These colored sections will be referred to in the following sections.
The drop-down menus highlighted in orange list additional features and utilities that make up the core functionality of the evaluation software.
- The Devices menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the ADIS16448 is selected.
- The Register Access option calls a sub-menu that lists all user-configurable registers available from the part number selected in the “Devices” drop-down menu. It also provides read/write access to each register.
- The Data Capture option calls a sub-menu designed to enable synchronous data logging from the selected device.
- The Demos option calls a 3-D visualization tool. This feature is only supported for the ADIS16480 and ADIS16448 devices.
- The Tools option calls a sub-menu that displays USB diagnostic information.
- The About option provides more detailed software revision information.
The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the Read button (identified by a red box).
The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, accelerometers, and magnetometers [if supported]). The top subplot displays gyroscope data, the middle plot displays accelerometer data and the bottom plot displays magnetometer data. Each plot color corresponds to the colors displayed in the “Output Registers” window (highlighted in purple).
The Register Access window provides read and write access to all user-accessible registers listed in the selected device's datasheet. The image below shows a screenshot of the window.
The color-coded image below is referenced in the following section.
The purple box sorts each set of registers into a standard category. The available categories are:
- Control/Status - General sensor configuration, alarm, and metadata registers
- Output - Inertial sensor output registers
- Calibration - User offset and misc. calibration registers
The section highlighted by the red box lists all of the registers in the selected category. Click on the register name to select a register for individual read/write access.
The green box identifies the read/write control options for the current register selection.
The Update Registers in Category button (shown in an orange box above) automatically reads all of the registers shown in the selected category (red box) and updates their contents in the GUI.
The section highlighted in yellow identifies provides a means of easily calling subroutines within the connected sensor. Clicking on a button is equivalent to writing a single-bit command to the respective register.
The Save Reg Settings to File programmatically reads and saves the contents of all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads a target .csv file and attempts to write the saved values back into the sensor.
The Data Capture window only supports synchronous data acquisition and logging to a file on the host PC. Data samples are only read from the sensor when the data ready pin toggles, indicating that data is valid.
The color-coded image below is referenced in the following section.
The section highlighted in red lists all of the registers that are eligible for data capture. Checking the box next to each register indicates that the specified register values should be recorded once the data stream begins.
The section highlighted in green allows for customizing the file name and location of the resultant .csv files.
The section highlighted in yellow identifies the data stream configuration options.
- Record Length - The total number of samples to be captured. A sample is defined as a single “data valid” period as signaled by the data ready pin on the sensor
- Sample Rate - The instantaneous data ready rate as measured by the evaluation board
- Capture Time - The estimated data capture time in DD:HH:MM:SS format calculated based upon the instantaneous sample rate
- Add File Header - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file
- Use Scaled Data - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/second
Click here to download the latest version of the IMU Evaluation software.
Click here to download the latest drivers for the EVAL-ADIS2.
The IMU Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to most ADIS16xxx products. This platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition, which is synchronous with data production of each ADIS16xxx.
Once the IMU Evaluation software loads, you should be presented with a window similar to the image shown below.
The image below has been color-coded to illustrate the different parts of the IMU Evaluation Software. These colored sections will be referred to in the following sections.
The drop-down menus highlighted in orange list additional features and utilities that make up the core functionality of the evaluation software.
- The Devices menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the ADIS16448 is selected.
- The Register Access option calls a sub-menu that lists all user-configurable registers available from the part number selected in the “Devices” drop-down menu. It also provides read/write access to each register.
- The Data Capture option calls a sub-menu designed to enable synchronous data logging from the selected device.
- The Demos option calls a 3-D visualization tool. This feature is only supported for the ADIS16480 and ADIS16448 devices.
- The Tools option calls a sub-menu that displays USB diagnostic information.
- The About option provides more detailed software revision information.
The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the Read button (identified by a red box).
The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, accelerometers, and magnetometers [if supported]). The top subplot displays gyroscope data, the middle plot displays accelerometer data and the bottom plot displays magnetometer data. Each plot color corresponds to the colors displayed in the “Output Registers” window (highlighted in purple).
The Register Access window provides read and write access to all user-accessible registers listed in the selected device's datasheet. The image below shows a screenshot of the window.
The color-coded image below is referenced in the following section.
The purple box sorts each set of registers into a standard category. The available categories are:
- Control/Status - General sensor configuration, alarm, and metadata registers
- Output - Inertial sensor output registers
- Calibration - User offset and misc. calibration registers
The section highlighted by the red box lists all of the registers in the selected category. Click on the register name to select a register for individual read/write access.
The green box identifies the read/write control options for the current register selection.
The Update Registers in Category button (shown in an orange box above) automatically reads all of the registers shown in the selected category (red box) and updates their contents in the GUI.
The section highlighted in yellow identifies provides a means of easily calling subroutines within the connected sensor. Clicking on a button is equivalent to writing a single-bit command to the respective register.
The Save Reg Settings to File programmatically reads and saves the contents of all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads a target .csv file and attempts to write the saved values back into the sensor.
The Data Capture window only supports synchronous data acquisition and logging to a file on the host PC. Data samples are only read from the sensor when the data ready pin toggles, indicating that data is valid.
The color-coded image below is referenced in the following section.
The section highlighted in red lists all of the registers that are eligible for data capture. Checking the box next to each register indicates that the specified register values should be recorded once the data stream begins.
The section highlighted in green allows for customizing the file name and location of the resultant .csv files.
The section highlighted in yellow identifies the data stream configuration options.
- Record Length - The total number of samples to be captured. A sample is defined as a single “data valid” period as signaled by the data ready pin on the sensor
- Sample Rate - The instantaneous data ready rate as measured by the evaluation board
- Capture Time - The estimated data capture time in DD:HH:MM:SS format calculated based upon the instantaneous sample rate
- Add File Header - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file
- Use Scaled Data - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/second
Edit the page and hit Save. See syntax for Wiki syntax. Please edit the page only if you can improve it. If you want to test some things, learn to make your first steps on the playground.
Click on the following links to access several useful experiments in ADI's Engineer Zone/MEMS Community.
Gyroscope Sensitivity Measurement