Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:imu:adis1646x [01 Feb 2016 18:01] – [SUMMARY] Mark Looneyresources:eval:user-guides:inertial-mems:imu:adis1646x [07 Apr 2023 17:56] (current) – [SETUP] Mark Looney
Line 3: Line 3:
  
 ===== OVERVIEW ===== ===== OVERVIEW =====
-Evaluating the [[adi>ADIS16460|ADIS16460]] on a PC requires the use of the [[adi>EVAL-ADIS16IMU4|ADIS16IMU4/PCBZ]] and [[adi>EVAL-ADIS|EVAL-ADIS]]. +Evaluating the [[adi>ADIS16460|ADIS16460]] and the AD24000 on a PC requires the use of the [[adi>EVAL-ADIS16IMU4|ADIS16IMU4/PCBZ]] and [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]]. Aside from this section of the datasheet, the instruction text and graphics identify only the ADIS16460.  However, all of these instructions apply to the AD24000 in the same manner.  Mention of AD24000 is omitted only to simplify the text
  
  
Line 17: Line 17:
  
  
-===== SETUP ===== +=====SETUP===== 
-The physical setup requires only three simple steps+The physical setup requires only three simple steps:
  
-Insert link from ADIS16IMU4/PCB Wiki Guide that describes installation of DUT onto breakout board+1. Install the DUT (for example, an ADIS16460AMLZ) onto the ADIS16IMU4/PCBZ 
 + 
 +2. Connect the ADIS16IMU4/PCBZ to the EVAL-ADIS-FX3Z 
 + 
 +3. Set JP1 Jumper on EVAL-ADIS-FX3Z 
 + 
 +====ADIS1646x Installation on the ADIS16IMU4/PCBZ==== 
 +{{page> resources/eval/user-guides/inertial-mems/imu/adis16imu4-pcb#dut_installation&nofooter&noheader}} 
 + 
 +====Connect the ADIS16IMU4/PCBZ to the EVAL-ADIS==== 
 +{{page> resources/eval/user-guides/inertial-mems/imu/adis16imu4-pcb#connecting_to_the_eval-adis&nofooter&noheader}}
  
-Insert link from ADIS16IMU4/PCB Wiki Guide that describes installation onto EVAL-ADIS 
  
-Insert link from EVAL-ADIS Wiki Guide that describes correct JP1 setting for DUT 
 ====IMU EVALUATION SOFTWARE OVERVIEW==== ====IMU EVALUATION SOFTWARE OVERVIEW====
  
Line 59: Line 67:
  
 ==== Gyroscope Demonstration ==== ==== Gyroscope Demonstration ====
-[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#gyroscope_demonstration|Click here to see a gyroscope demonstration, from the ADIS16448 Wiki Site]].+[[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#gyroscope_demonstration|Click here to see a gyroscope demonstration, from the ADIS16448 Wiki Site]].
  
 ==== Accelerometer Demonstration, Static ==== ==== Accelerometer Demonstration, Static ====
-[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_gravity|Click here to see the static (gravity) accelerometer demonstration, from the ADIS16448 Wiki Site]].+[[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_gravity|Click here to see the static (gravity) accelerometer demonstration, from the ADIS16448 Wiki Site]].
  
 ==== Accelerometer Demonstration, Dynamic ==== ==== Accelerometer Demonstration, Dynamic ====
-[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_dynamic|Click here to see the dynamic accelerometer demonstration, from the ADIS16448 Wiki Site]].+[[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#accelerometer_demonstration_dynamic|Click here to see the dynamic accelerometer demonstration, from the ADIS16448 Wiki Site]].
  
 ==== Useful Experiments ==== ==== Useful Experiments ====
 Click on the following links to access several useful experiments in ADI's Engineer Zone/MEMS Community. Click on the following links to access several useful experiments in ADI's Engineer Zone/MEMS Community.
  
-[[http://ez.analog.com/docs/DOC-2181|Gyroscope Sensitivity Measurement]]+[[ez>docs/DOC-2181|Gyroscope Sensitivity Measurement]]
  
-[[http://ez.analog.com/docs/DOC-2212|Gyroscope Noise Density]]+[[ez>docs/DOC-2212|Gyroscope Noise Density]]
  
-[[http://ez.analog.com/docs/DOC-2162|Gyroscope In-Run Bias Stability]]+[[ez>docs/DOC-2162|Gyroscope In-Run Bias Stability]]
  
-[[http://ez.analog.com/docs/DOC-2163|Gyroscope Angle Random Walk]]+[[ez>docs/DOC-2163|Gyroscope Angle Random Walk]]
  
-[[http://ez.analog.com/docs/DOC-2223|ADIS16480 3-D Demonstration]]+[[ez>docs/DOC-2223|ADIS16480 3-D Demonstration]]
  
  
resources/eval/user-guides/inertial-mems/imu/adis1646x.1454346109.txt.gz · Last modified: 01 Feb 2016 18:01 by Mark Looney