Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:imu:adis1646x [09 Jan 2021 00:39] – user interwiki links Robin Getzresources:eval:user-guides:inertial-mems:imu:adis1646x [07 Apr 2023 17:56] (current) – [SETUP] Mark Looney
Line 3: Line 3:
  
 ===== OVERVIEW ===== ===== OVERVIEW =====
-Evaluating the [[adi>ADIS16460|ADIS16460]] and the AD24000 on a PC requires the use of the [[adi>EVAL-ADIS16IMU4|ADIS16IMU4/PCBZ]] and [[adi>EVAL-ADIS|EVAL-ADIS]]. Aside from this section of the datasheet, the instruction text and graphics identify only the ADIS16460.  However, all of these instructions apply to the AD24000 in the same manner.  Mention of AD24000 is omitted only to simplify the text. +Evaluating the [[adi>ADIS16460|ADIS16460]] and the AD24000 on a PC requires the use of the [[adi>EVAL-ADIS16IMU4|ADIS16IMU4/PCBZ]] and [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]]. Aside from this section of the datasheet, the instruction text and graphics identify only the ADIS16460.  However, all of these instructions apply to the AD24000 in the same manner.  Mention of AD24000 is omitted only to simplify the text. 
  
  
Line 22: Line 22:
 1. Install the DUT (for example, an ADIS16460AMLZ) onto the ADIS16IMU4/PCBZ 1. Install the DUT (for example, an ADIS16460AMLZ) onto the ADIS16IMU4/PCBZ
  
-2. Connect the ADIS16IMU4/PCBZ to the EVAL-ADISZ+2. Connect the ADIS16IMU4/PCBZ to the EVAL-ADIS-FX3Z
  
-3. Set JP1 Jumper on EVAL-ADISZ+3. Set JP1 Jumper on EVAL-ADIS-FX3Z
  
 ====ADIS1646x Installation on the ADIS16IMU4/PCBZ==== ====ADIS1646x Installation on the ADIS16IMU4/PCBZ====
resources/eval/user-guides/inertial-mems/imu/adis1646x.txt · Last modified: 07 Apr 2023 17:56 by Mark Looney