Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:inertial-mems:imu:adis16375-adisusb [29 Apr 2015 15:40] – [PHYSICAL SETUP] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16375-adisusb [29 Apr 2015 15:44] – [PHYSICAL SETUP] Mark Looney |
---|
NOTE: Do not plug the [[adi>ADISUSB|ADISUSB]] into the USB cable at this stage of the setup. Wait until the software installation is complete. | NOTE: Do not plug the [[adi>ADISUSB|ADISUSB]] into the USB cable at this stage of the setup. Wait until the software installation is complete. |
| |
=== Step #1 === | ==== Step #1 ==== |
The [[adi>ADIS16375|ADIS16375AMLZ]] installs directly into the J4 connector of the [[adi>ADISUSB|ADISUSB]]. The following pictures provide a visual reference for correct connection. Mounting to the system frame is accomplished by Drilling and tapping for M2 (drill size #52 1.6mm) or 2-56 (drill size #50 .070) holes in the [[adi>ADISUSB|ADISUSB]], according to the locations in the physical mounting diagram. The tap is the best way but an M2x0.4 machine screw can be used for tapping the PCB material. The [[adi>ADIS16375|ADIS16375AMLZ]] is secured using the M2x0.4x18mm machine screws included with the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]. The mounting location holes are shown in the picture below. | The [[adi>ADIS16375|ADIS16375AMLZ]] installs directly into the J4 connector of the [[adi>ADISUSB|ADISUSB]]. The following pictures provide a visual reference for correct connection. Mounting to the system frame is accomplished by Drilling and tapping for M2 (drill size #52 1.6mm) or 2-56 (drill size #50 .070) holes in the [[adi>ADISUSB|ADISUSB]], according to the locations in the physical mounting diagram. The tap is the best way but an M2x0.4 machine screw can be used for tapping the PCB material. The [[adi>ADIS16375|ADIS16375AMLZ]] is secured using the M2x0.4x18mm machine screws included with the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]. The mounting location holes are shown in the picture below. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:375-correct-j4-connection.png?600 |}} | {{:resources:eval:user-guides:inertial-mems:imu:375-correct-j4-connection.png?600 |}} |
| |
=== Step #2 === | ==== Step #2 ==== |
The remote mounting option [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]] includes one [[adi>ADIS16375|ADIS16375AMLZ]], one interface printed circuit board (PCB), and four M2 × 0.4 x 18mm machine screws. The interface PCB provides larger connectors than the [[adi>ADIS16375|ADIS16375AMLZ]] for simpler prototyping, four-tapped M2 holes for attachment of the [[adi>ADIS16375|ADIS16375AMLZ]], and four holes (machine screw size M2.5 or #4) for mounting the [[adi>ADIS16375|ADIS16375AMLZ]] to a solid structure. J1 is a dual-row, 2 mm (pitch) connector that mates to a number of ribbon cable systems, including 3M Part Number 152212-0100-GB (ribbon crimp connector) and 3M Part Number 3625/12 (ribbon cable). Note that J1 has 16 pads; however, some legacy boards use only Pin 1 through Pin 12. | The remote mounting option [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]] includes one [[adi>ADIS16375|ADIS16375AMLZ]], one interface printed circuit board (PCB), and four M2 × 0.4 x 18mm machine screws. The interface PCB provides larger connectors than the [[adi>ADIS16375|ADIS16375AMLZ]] for simpler prototyping, four-tapped M2 holes for attachment of the [[adi>ADIS16375|ADIS16375AMLZ]], and four holes (machine screw size M2.5 or #4) for mounting the [[adi>ADIS16375|ADIS16375AMLZ]] to a solid structure. J1 is a dual-row, 2 mm (pitch) connector that mates to a number of ribbon cable systems, including 3M Part Number 152212-0100-GB (ribbon crimp connector) and 3M Part Number 3625/12 (ribbon cable). Note that J1 has 16 pads; however, some legacy boards use only Pin 1 through Pin 12. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:375-mounted-on-pcbz-brd.png?400}} | {{:resources:eval:user-guides:inertial-mems:imu:375-mounted-on-pcbz-brd.png?400}} |
| |
=== Step #3 === | ==== Step #3 ==== |
Secure the [[adi>ADIS16375|ADIS16375AMLZ]] body, to the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]] using (4) M2x0.4x18mm machine screws (included with [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]). The suggested torque setting for the attachment hardware is 40 inch-ounces, or 0.2825 N-m. | Secure the [[adi>ADIS16375|ADIS16375AMLZ]] body, to the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]] using (4) M2x0.4x18mm machine screws (included with [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]). The suggested torque setting for the attachment hardware is 40 inch-ounces, or 0.2825 N-m. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:375-adisusb-16375pcbz2.png?400}} | {{:resources:eval:user-guides:inertial-mems:imu:375-adisusb-16375pcbz2.png?400}} |
| |
=== Step #4 === | ==== Step #4 ==== |
Connect J1 on the [[adi>ADISUSB|ADISUSB]] to J1 on the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]. Note that J1 ([[adi>ADISUSB|ADISUSB]]) has 12 pins and J1 ([[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]) has 16 pins. The four DIO pins are left un-connected using the 12 pin connector which allows easy access and shown in the pictures below. | Connect J1 on the [[adi>ADISUSB|ADISUSB]] to J1 on the [[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]. Note that J1 ([[adi>ADISUSB|ADISUSB]]) has 12 pins and J1 ([[adi>en/mems-sensors/mems-inertial-measurement-units/adis16375/products/EVAL-ADIS16375/eb.html|ADIS16375/PCBZ]]) has 16 pins. The four DIO pins are left un-connected using the 12 pin connector which allows easy access and shown in the pictures below. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:375-adisusb-16375pcbz4.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:375-adisusb-16375pcbz4.png?400|}} |
| |
=== Step #5 === | ==== Step #5 ==== |
The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). If this is different, change the JP1 jumper setting on the [[adi>ADISUSB|ADISUSB]] to the **+3.3V** position and shown in the following picture: | The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). If this is different, change the JP1 jumper setting on the [[adi>ADISUSB|ADISUSB]] to the **+3.3V** position and shown in the following picture: |
| |