Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16227-adisusb [08 Oct 2013 03:41] – [USB Driver Installation] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16227-adisusb [27 Jan 2021 22:34] (current) – use wp> interwiki links Robin Getz |
---|
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} |
| |
<wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. Please see page 8, on the **[[http://www.analog.com/static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap> | <wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. Please see page 8, on the **[[adi>static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap> |
===== ADIS16227 Evaluation SOFTWARE ===== | ===== ADIS16227 Evaluation SOFTWARE ===== |
After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the ADiS16227_Eval_Rev_2.exe file to launch the software application. | After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the ADiS16227_Eval_Rev_2.exe file to launch the software application. |
| |
The green box identifies the configuration box for the name and location of the data storage file. | The green box identifies the configuration box for the name and location of the data storage file. |
The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value. For example, when enabling **Use Scaled Data,** the accelerometer outputs will be in units of g's [[http://en.wikipedia.org/wiki/G-force|g-force]]. | The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value. For example, when enabling **Use Scaled Data,** the accelerometer outputs will be in units of g's [[wp>G-force|g-force]]. |
| |
==== EXAMPLE EXERCISES ==== | ==== EXAMPLE EXERCISES ==== |
This section currently has no [[adi>ADIS16227|ADIS16227]]-specific content, but the | This section currently has no [[adi>ADIS16227|ADIS16227]]-specific content, but the |
[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. |