This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:inertial-mems:imu:adis16227-adisusb [09 Jan 2021 00:39] Robin Getz user interwiki links |
resources:eval:user-guides:inertial-mems:imu:adis16227-adisusb [27 Jan 2021 22:34] Robin Getz use wp> interwiki links |
||
---|---|---|---|
Line 198: | Line 198: | ||
The green box identifies the configuration box for the name and location of the data storage file. | The green box identifies the configuration box for the name and location of the data storage file. | ||
- | The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value. For example, when enabling **Use Scaled Data,** the accelerometer outputs will be in units of g's [[http://en.wikipedia.org/wiki/G-force|g-force]]. | + | The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value. For example, when enabling **Use Scaled Data,** the accelerometer outputs will be in units of g's [[wp>G-force|g-force]]. |
==== EXAMPLE EXERCISES ==== | ==== EXAMPLE EXERCISES ==== | ||
This section currently has no [[adi>ADIS16227|ADIS16227]]-specific content, but the | This section currently has no [[adi>ADIS16227|ADIS16227]]-specific content, but the | ||
[[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. | [[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. |