Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:inertial-mems:imu:adis16210-pcb [06 Jul 2016 21:39] – [USE WITH THE EVAL-ADIS SYSTEM] Mark Looneyresources:eval:user-guides:inertial-mems:imu:adis16210-pcb [07 Jul 2016 04:26] (current) – [ELECTRICAL SCHEMATIC] Mark Looney
Line 8: Line 8:
 =====INTERFACE PCB===== =====INTERFACE PCB=====
 The interface PCB provides access to the ADIS16210CMLZ, using a dual-row, 16-pin connector, which supports standard ribbon cable systems and hand-soldering connection techniques. The interface PCB also provides two sets of mounting holes: one set of holes for attaching the ADIS16210CMLZ to the interface PCB and another set of holes for mounting the interface board to the system’s frame. The first set of holes line up with the ADIS16210CMLZ's mounting holes and are pre-tapped for use with M2x0.4mm machine screws. The second set of holes are support M2 machine screws and line up with M2x0.4mm, pre-tapped holes on the EVAL-ADIS evaluation system board.  The interface PCB provides access to the ADIS16210CMLZ, using a dual-row, 16-pin connector, which supports standard ribbon cable systems and hand-soldering connection techniques. The interface PCB also provides two sets of mounting holes: one set of holes for attaching the ADIS16210CMLZ to the interface PCB and another set of holes for mounting the interface board to the system’s frame. The first set of holes line up with the ADIS16210CMLZ's mounting holes and are pre-tapped for use with M2x0.4mm machine screws. The second set of holes are support M2 machine screws and line up with M2x0.4mm, pre-tapped holes on the EVAL-ADIS evaluation system board. 
-====ELECTRICAL SCHEMATIC====+====Mechanical Drawing==== 
 + 
 +{{:resources:eval:user-guides:inertial-mems:imu:adis16210_pcbz_wiki_02.png?600|}} 
 + 
 +====Electrical Schematic====
 Please see the following graphic for the Interface PCB's electrical schematic: Please see the following graphic for the Interface PCB's electrical schematic:
  
resources/eval/user-guides/inertial-mems/imu/adis16210-pcb.txt · Last modified: 07 Jul 2016 04:26 by Mark Looney