Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:gyroscopes:adis1613x-adisusb [27 Aug 2020 22:46]
Juan Chong Cleaned up summary
resources:eval:user-guides:inertial-mems:gyroscopes:adis1613x-adisusb [09 Jan 2021 00:39] (current)
Robin Getz user interwiki links
Line 27: Line 27:
 {{:​resources:​eval:​user-guides:​inertial-mems:​imu:​adisusb-driver-complete-wizard.png?​400|}} {{:​resources:​eval:​user-guides:​inertial-mems:​imu:​adisusb-driver-complete-wizard.png?​400|}}
  
-<note important>​For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. ​ Please see page 8, on the **[[http://​www.analog.com/​static/​imported-files/​user_guides/​UG-363.pdf#​Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps.</​note>​+<note important>​For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. ​ Please see page 8, on the **[[adi>static/​imported-files/​user_guides/​UG-363.pdf#​Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps.</​note>​
  
 After the USB driver installation is complete, connect the [[adi>​ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>​ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>​ADISUSB|ADISUSB]] has power and is going through its start-up/​initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>​ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>​ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application. After the USB driver installation is complete, connect the [[adi>​ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>​ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>​ADISUSB|ADISUSB]] has power and is going through its start-up/​initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>​ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>​ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application.
Line 48: Line 48:
  
 ==== Register Access ==== ==== Register Access ====
-The purpose of the **Register Access** window is to provide both read and write access to the user registers in the [[adi>ADIS1613x|ADIS1613x]]. The following picture shows the appearance of this window.+The purpose of the **Register Access** window is to provide both read and write access to the user registers in the [[adi>ADIS16136|ADIS1613x]]. The following picture shows the appearance of this window.
  
 {{:​resources:​eval:​user-guides:​inertial-mems:​gyroscopes:​13x-adisusb-registers.png?​600|}} {{:​resources:​eval:​user-guides:​inertial-mems:​gyroscopes:​13x-adisusb-registers.png?​600|}}
resources/eval/user-guides/inertial-mems/gyroscopes/adis1613x-adisusb.1598561208.txt.gz · Last modified: 27 Aug 2020 22:46 by Juan Chong