Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:inertial-mems:gyroscopes:adis1613x-adisusb [08 Jan 2021 09:43]
Ioana Chelaru Fixed bad link for ADIS16136
resources:eval:user-guides:inertial-mems:gyroscopes:adis1613x-adisusb [09 Jan 2021 00:39]
Robin Getz user interwiki links
Line 27: Line 27:
 {{:​resources:​eval:​user-guides:​inertial-mems:​imu:​adisusb-driver-complete-wizard.png?​400|}} {{:​resources:​eval:​user-guides:​inertial-mems:​imu:​adisusb-driver-complete-wizard.png?​400|}}
  
-<note important>​For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. ​ Please see page 8, on the **[[http://​www.analog.com/​static/​imported-files/​user_guides/​UG-363.pdf#​Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps.</​note>​+<note important>​For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. ​ Please see page 8, on the **[[adi>static/​imported-files/​user_guides/​UG-363.pdf#​Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps.</​note>​
  
 After the USB driver installation is complete, connect the [[adi>​ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>​ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>​ADISUSB|ADISUSB]] has power and is going through its start-up/​initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>​ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>​ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application. After the USB driver installation is complete, connect the [[adi>​ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>​ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>​ADISUSB|ADISUSB]] has power and is going through its start-up/​initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>​ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>​ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application.
resources/eval/user-guides/inertial-mems/gyroscopes/adis1613x-adisusb.txt · Last modified: 09 Jan 2021 00:39 by Robin Getz