This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:inertial-mems:gyroscopes:adis16130-eval-adis [09 Jan 2021 00:39] – user interwiki links Robin Getz | resources:eval:user-guides:inertial-mems:gyroscopes:adis16130-eval-adis [11 Feb 2021 17:55] (current) – Ioana Chelaru | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== ADIS16130 EVALUATION ON THE EVAL-ADIS ===== | + | f===== ADIS16130 EVALUATION ON THE EVAL-ADIS ===== |
==== INTRODUCTION ==== | ==== INTRODUCTION ==== | ||
The purpose of this Wiki Guide is to describe an approach to use for evaluating the [[adi> | The purpose of this Wiki Guide is to describe an approach to use for evaluating the [[adi> | ||
Line 204: | Line 204: | ||
- | Take note of the clamps that are on the interface board, but not on the [[adi> | + | Take note of the clamps that are on the interface board, but not on the [[adi> |
The following table illustrates the thermal profile for the temperature chamber for this experiment. For those who are developing calibration systems, the dwell times and ramp rates are likely to be an area for application-specific optimization. | The following table illustrates the thermal profile for the temperature chamber for this experiment. For those who are developing calibration systems, the dwell times and ramp rates are likely to be an area for application-specific optimization. |