Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis2 [19 Dec 2017 14:46] – [EVAL-ADIS2 Kit Contents] Mark Looney | resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis2 [19 Dec 2017 14:53] – [Step #2: DUT/Breakout Board Connection] Mark Looney |
---|
====Step #2: DUT/Breakout Board Connection==== | ====Step #2: DUT/Breakout Board Connection==== |
| |
All ADIS16xxx (DUT) devices connect to the [[adi>EVAL-ADIS2|EVAL-ADIS2]] through a **__breakout board__**. There are two different types of breakout boards: __Model-specific__ and __Generic__. __Model-specific__ breakout boards typically support products that require solder-reflow attachment, while __Generic__ breakout boards typically support products that use some form of "press-in" connectors. So, the __Model-specific__ breakout boards typically come have their DUT already installed onto the board, while the __Generic__ breakout boards do not include the DUT (they have to be purchased separately). | All ADIS16xxx (DUT) devices connect to the [[adi>EVAL-ADIS2|EVAL-ADIS2]] through a **__breakout board__**. There are two different types of breakout boards: __Model-specific__ and __Generic__. |
| |
| __Model-specific__ breakout boards typically support products that require solder-reflow attachment, while __Generic__ breakout boards typically support products that use some form of "press-in" connectors. So, the __Model-specific__ breakout boards typically come have their DUT already installed onto the board, while the __Generic__ breakout boards do not include the DUT (they have to be purchased separately). |
| |
The following table provides a summary of the most appropriate breakout board for each ADIS16xxx device, which uses a __Generic__ breakout board to connect with the [[adi>EVAL-ADIS2|EVAL-ADIS2]]. **TIP:** Hover the mouse pointer over the breakout board (heading row in the table), right click on it, then click on **Open in new tab** to open useful setup instructions for that breakout board, in a new tab. | The following table provides a summary of the most appropriate breakout board for each ADIS16xxx device, which uses a __Generic__ breakout board to connect with the [[adi>EVAL-ADIS2|EVAL-ADIS2]]. **TIP:** Hover the mouse pointer over the breakout board (heading row in the table), right click on it, then click on **Open in new tab** to open useful setup instructions for that breakout board, in a new tab. |