This shows you the differences between two versions of the page.
— | resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis2 [03 Jul 2018 21:29] – [Dimensions/Hole Locations] Mark Looney | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== EVAL-ADIS2 EVALUATION SYSTEM ====== | ||
+ | The [[adi> | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The following picture identifies the key features associated with this evaluation system. Click on the image to access a larger view. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | For a complete listing of products that the [[adi> | ||
+ | |||
+ | =====EVAL-ADIS2 Kit Contents===== | ||
+ | - EVAL-ADIS2 Evaluation Board | ||
+ | |||
+ | - Mini USB Cable, 6ft | ||
+ | |||
+ | - 16-pin IDC cable, 1.5" | ||
+ | |||
+ | - 16-pin IDC cable, 12" | ||
+ | |||
+ | - M2x0.4mm machine screw/ | ||
+ | | ||
+ | **NOTE:** The [[adi> | ||
+ | ===== PC System Requirements ===== | ||
+ | - Microsoft Windows | ||
+ | |||
+ | - ADI SDP USB Driver | ||
+ | |||
+ | -.NET Framework 3.5 | ||
+ | |||
+ | |||
+ | ===== Quick Start Guide ===== | ||
+ | The following sequence of steps provides the quickest and most reliable process for setting up your **EVAL-ADIS2** for operation on a PC. | ||
+ | |||
+ | ====Step #1: DUT Supply Setting==== | ||
+ | |||
+ | JP1 provides three DUT power supply options: **+3.3V**, **+5V** and **Ext** (external supply). | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Use the following table to identify the correct JP1 setting for the DUT: | ||
+ | |||
+ | ^ JP1 = +3.3V ^ JP1 = +5V ^ | ||
+ | |ADIS16201, ADIS16203, ADIS16209, ADIS16210, ADIS16223, ADIS16227, ADIS16228, ADIS16375, ADIS16445, ADIS16448, ADIS16460, ADIS16465, ADIS16467, ADIS16470, ADIS16475, ADIS16477, ADIS16480, ADIS16485, ADIS16488A, ADIS16490, ADIS16495, ADIS16497| ADIS16133, ADIS16135, ADIS16136, ADIS16137, ADIS16260, ADIS16265, ADIS16266, ADIS16300, ADIS16305, ADIS16334, ADIS16360, ADIS16362, ADIS16365, ADIS16367, ADIS16400, ADIS16405, ADIS16407| | ||
+ | |||
+ | __External Supply Option__ | ||
+ | |||
+ | In order to use external supply option, remove the header from **JP1** and solder the middle post to the hole that has the **EXT** label on the **EVAL-ADIS2**. The next revision of this board will move this hole so that this option will be available using the same header that connects to the **+3.3V** and **+5V** settings on **JP1**. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Then, connect the external supply to J3, using the following diagram to illustrate the correct connections: | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ====Step #2: DUT/ | ||
+ | |||
+ | All ADIS16xxx (DUT) devices connect to the [[adi> | ||
+ | |||
+ | __Model-specific__ breakout boards typically support products that require solder-reflow attachment, while __Generic__ breakout boards typically support products that use some form of " | ||
+ | |||
+ | The following table provides a summary of the most appropriate breakout board for each ADIS16xxx device, which uses a __Generic__ breakout board to connect with the [[adi> | ||
+ | |||
+ | ^[[resources/ | ||
+ | |ADIS16133 ADIS16135 ADIS16136 ADIS16137 ADIS16375 ADIS16480 ADIS16485 ADIS16488A ADIS16490 ADIS16495 ADIS16497|ADIS16360 ADIS16362 ADIS16364 ADIS16365 ADIS16367 ADIS16400 ADIS16405 ADIS16407|ADIS16334 ADIS16445 ADIS16448 |ADIS16460 ADIS16465 ADIS16467|ADIS16210 ADIS16228 |ADIS16223 ADIS16227 | | ||
+ | ====Step #3: Breakout Board/ | ||
+ | |||
+ | The J1 connector on the [[adi> | ||
+ | |||
+ | {{: | ||
+ | {{: | ||
+ | |||
+ | NOTE: The supporting connector (J1) on the ADIS1620x/ | ||
+ | |||
+ | [[resources/ | ||
+ | ====Step #4: USB Driver==== | ||
+ | |||
+ | Download the USB driver for the EVAL-ADIS2 and store it in a convenient, temporary folder on the Test PC. Then, double click on this file. Answer all of the questions presented by the installation routine. | ||
+ | |||
+ | [[http:// | ||
+ | |||
+ | After downloading the EVAL-ADIS USB Driver file, extract the SDPDrivers.exe file from the zip file, into a convenient location and then double click on it to start the process. When the setup wizard opens, click on **Next** to start the installation process | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Click on **Next** to accept the default driver location. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | The process will involve at least two progress bars that look like the following: | ||
+ | |||
+ | {{: | ||
+ | |||
+ | If you encounter this type of message during the process, click on **Install** to continue with the installation. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Once the installation has completed, click on **Finish** to complete the process. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ====Step #5: Application Software==== | ||
+ | |||
+ | Download the DUT's evaluation software package, but clicking on its heading in the following table. Store the file in a convenient location on the test PC and extract its executable file. | ||
+ | |||
+ | ^[[http:// | ||
+ | |ADIS16133, ADIS16135, ADIS16136, ADIS16137, ADIS16201, ADIS16203, ADIS16260, ADIS16265, ADIS16266, ADIS16334, ADIS16360, ADIS16362, ADIS16364, ADIS16365, ADIS16367, ADIS16375, ADIS16400, ADIS16405, ADIS16407, ADIS16445, ADIS16448, ADIS16460, ADIS16465, ADIS16467, ADIS16470, ADIS16475, ADIS16477, ADIS16480, ADIS16485, ADIS16488A, ADIS16490, ADIS16495, ADIS16497|ADIS16227, | ||
+ | |||
+ | ====Step #6: PC/ | ||
+ | |||
+ | Use a Mini USB cable to connect J2 (Mini USB connector) to a USB port on the PC. LED2 will light up very quickly and LED1 will take as long as 10 seconds to illuminate. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ====Step #7: Start Evaluation Software==== | ||
+ | |||
+ | Double click on the executable file to launch the application software. | ||
+ | |||
+ | __IMU Evaluation Software__ | ||
+ | |||
+ | Please visit the [[https:// | ||
+ | |||
+ | **Coming soon:** Update to include latest version | ||
+ | |||
+ | __Vibration Evaluation Software__ | ||
+ | |||
+ | Please visit the [[https:// | ||
+ | |||
+ | **Coming soon:** Update to include latest version | ||
+ | |||
+ | =====Product Tutorials===== | ||
+ | |||
+ | **Coming soon:** Product-specific tutorials, tips and tricks | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ===== Tool Cross Reference Guide ===== | ||
+ | The following table provides a list of products that the EVAL-ADIS2 supports, along with the appropriate breakout board, JP1 setting and software package for each of these products. | ||
+ | ^ MODEL NUMBER ^ BREAKOUT BOARD ^ JP1 SETTING ^ SOFTWARE PACKAGE ^ | ||
+ | |ADIS16133BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16135BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16136BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16137BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16201CCCZ |ADIS16201/ | ||
+ | |ADIS16203CCCZ |ADIS16203/ | ||
+ | |ADIS16209CCCZ |ADIS16209/ | ||
+ | |ADIS16210BMLZ |ADIS16ACL1/ | ||
+ | |ADIS16223CMLZ |ADIS16ACL2/ | ||
+ | |ADIS16227CMLZ |ADIS16ACL2/ | ||
+ | |ADIS16228BMLZ |ADIS16ACL1/ | ||
+ | |ADIS16265BCCZ |ADIS16265/ | ||
+ | |ADIS16334BMLZ |ADIS16IMU2/ | ||
+ | | |ADIS1644X/ | ||
+ | |ADIS16362BMLZ |ADIS16IMU2/ | ||
+ | |ADIS16364BMLZ |ADIS16IMU2/ | ||
+ | |ADIS16365BMLZ |ADIS16IMU2/ | ||
+ | |ADIS16367BMLZ |ADIS16IMU2/ | ||
+ | |ADIS16375BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16405BMLZ |ADIS16IMU2/ | ||
+ | |ADIS16407BMLZ |ADIS16IMU2/ | ||
+ | |ADIS16445BMLZ |ADIS16IMU2/ | ||
+ | | |ADIS1644X/ | ||
+ | |ADIS16448BMLZ |ADIS16IMU2/ | ||
+ | | |ADIS1644X/ | ||
+ | |ADIS16460AMLZ |ADIS16IMU4/ | ||
+ | |ADIS16465-1BMLZ |ADIS16IMU4/ | ||
+ | |ADIS16465-2BMLZ |ADIS16IMU4/ | ||
+ | |ADIS16465-3BMLZ |ADIS16IMU4/ | ||
+ | |ADIS16467-1BMLZ |ADIS16IMU4/ | ||
+ | |ADIS16467-2BMLZ |ADIS16IMU4/ | ||
+ | |ADIS16467-3BMLZ |ADIS16IMU4/ | ||
+ | |ADIS16470AMLZ |ADIS16470/ | ||
+ | |ADIS16475-1BMLZ |ADIS16475-1/ | ||
+ | |ADIS16475-2BMLZ |ADIS16475-2/ | ||
+ | |ADIS16475-3BMLZ |ADIS16475-3/ | ||
+ | |ADIS16477-1BMLZ |ADIS16477-1/ | ||
+ | |ADIS16477-2BMLZ |ADIS16477-2/ | ||
+ | |ADIS16477-3BMLZ |ADIS16477-3/ | ||
+ | |ADIS16480BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16485BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16488BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16488CMLZ |ADIS16IMU1/ | ||
+ | |ADIS16490BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16495-1BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16495-2BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16495-3BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16497-1BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16497-2BMLZ |ADIS16IMU1/ | ||
+ | |ADIS16497-3BMLZ |ADIS16IMU1/ | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ===== Dimensions/ | ||
+ | |||
+ | Here is a top-level view of the key physical dimensions in the EVAL-ADIS2 board | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Please click on the following file for a PDF version of this drawing: | ||
+ | {{ : | ||
+ | |||
+ | |||
+ | ===== J1 Pin Assignments ===== | ||
+ | |||
+ | Here are the pin assignments for J1, which is the connector that will interface with all of the ADIS16xxx breakout boards. | ||
+ | |||
+ | {{: | ||
+ | ===== System Requirements ===== | ||
+ | The EVAL-ADIS2 is compatible with most PCs that run Windows operating systems. | ||
+ | |||
+ | ===== Ordering ===== | ||
+ | [[adi> | ||
+ | |||
+ | ===== Development Support ===== | ||
+ | No official support | ||
+ | Limited, please feel free to try these examples out. | ||
+ | |||