This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:evalsystem:installdrivers [15 Jan 2013 21:28] – created Nitzan Gadish | resources:eval:user-guides:inertial-mems:evalsystem:installdrivers [18 Jan 2013 04:30] (current) – [How to Install Drivers (Without an Installer)] Nitzan Gadish | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== How to Find Your COM Port ====== | + | ====== How to Install Drivers (Without an Installer) |
- | This page describes how to determine which COM port is being used for communication with your Analog Devices Inertial Sensor Evaluation System. | + | This page describes how to install drivers without an installer, as in the case of the [[resources: |
- | <WRAP tip>Use the Table of Contents on the right to jump to instructions for your operating system.</ | + | <WRAP tip>Use the Table of Contents on the right to scroll |
+ | Note that your system may behave slightly differently, | ||
===== Windows 7 ===== | ===== Windows 7 ===== | ||
- Connect the board to your computer via a USB cable. | - Connect the board to your computer via a USB cable. | ||
- | - If prompted to install drivers | + | - If prompted to install drivers, choose **Install from a list or specific location (Advanced)**, |
- | - Select | + | - Click the Windows button in the bottom left corner of the screen to open the Start menu. |
- | - Select | + | - Right-click on **My Computer**, and select **Manage**. In the warning screen that comes up, click **Yes**. |
- | - Click **Have Disk...**. On the screen that opens, select **Browse...** | + | - In the window that opens, select the **Device Manager** from the list on the left-hand side. |
- | - Click **Open**, then in the **Install From Disk** prompt, click **OK**. | + | - The board will show up in the Device Manager as an **Unknown Device**. (If it shows up under **Ports (COM & LPT)** |
- | - Select "ADI Inertial Sensor Development Board" in the **Model** list, and click **Next >**. | + | - Right-click on the Unknown Device and select **Update Driver Installation...**. Follow the remaining instructions below. |
- | - Respond **Continue Anyway** to the warning. | + | </ |
- | - Click **Finish** to complete the USB driver installation. | + | - Select **Let me pick...**, then click **Next**. |
- | - | + | {{: |
- | ===== Windows Vista ===== | + | - Select **Show All Devices**, and click **Next**.< |
+ | {{: | ||
+ | - Click **Have Disk...**. | ||
+ | {{: | ||
+ | - On the screen that opens, select **Browse...** | ||
+ | {{: | ||
+ | - Navigate | ||
+ | {{: | ||
+ | - Click **Open**, then in the **Install From Disk** prompt, click **OK**. | ||
+ | {{: | ||
+ | - Select "ADI Inertial Sensor Development Board" in the **Model** list, and click **Next > | ||
+ | </ | ||
+ | - Respond **Continue Anyway** or **Install** to the warning. | ||
+ | {{: | ||
+ | - Click **Close** to complete the USB driver installation. | ||
+ | {{: | ||
+ | |||
+ | ---- | ||
+ | |||
+ | |||
Line 24: | Line 45: | ||
- Connect the board to your computer via a USB cable. | - Connect the board to your computer via a USB cable. | ||
- | - If prompted to install drivers | + | - When prompted to install drivers, choose **Install from a list or specific location (Advanced)**, |
- | - Select **Don' | + | {{: |
- | - Select **Ports (COM & LPT)**, and click **Next**. | + | - Select **Don' |
- | - Click **Have Disk...**. On the screen that opens, select **Browse...** | + | {{: |
- | - Click **Open**, then in the **Install From Disk** prompt, click **OK**. | + | - Select **Ports (COM & LPT)**, and click **Next**. |
- | - Select "ADI Inertial Sensor Development Board" in the **Model** list, and click **Next >**. | + | {{: |
- | - Respond **Continue Anyway** to the warning. | + | - Click **Have Disk...**. |
- | - Click **Finish** to complete the USB driver installation. | + | {{: |
+ | - On the screen that opens, select **Browse...**. <WRAP indent> | ||
+ | {{: | ||
+ | - Navigate | ||
+ | {{: | ||
+ | - Click **Open**, then in the **Install From Disk** prompt, click **OK**.<WRAP indent> | ||
+ | {{: | ||
+ | - Select "ADI Inertial Sensor Development Board" in the **Model** list, and click **Next > | ||
+ | {{: | ||
+ | - Respond **Continue Anyway** to the warning. | ||
+ | {{: | ||
+ | - Click **Finish** to complete the USB driver installation. | ||
+ | {{: |