This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:accelerometers:inclinometer-app [28 Jul 2022 05:27] Jipcy Narvaez |
resources:eval:user-guides:inertial-mems:accelerometers:inclinometer-app [29 Jul 2022 04:31] Jipcy Narvaez |
||
---|---|---|---|
Line 9: | Line 9: | ||
* Can simulate Single Axis or Dual Axis Inclinometer | * Can simulate Single Axis or Dual Axis Inclinometer | ||
* Includes different ADXL Devices with digital interface | * Includes different ADXL Devices with digital interface | ||
- | * * [[adi>ADXL312]] , [[adi>ADXL313]] , [[adi>ADXL314]] , | + | * * [[adi>ADXL312]] , [[adi>ADXL313]] , [[adi>ADXL343]] , |
* * [[adi>ADXL344]] , [[adi>ADXL345]] , [[adi>ADXL346]] , | * * [[adi>ADXL344]] , [[adi>ADXL345]] , [[adi>ADXL346]] , | ||
* * [[adi>ADXL350]] , [[adi>ADXL355]] , [[adi>ADXL362]] , | * * [[adi>ADXL350]] , [[adi>ADXL355]] , [[adi>ADXL362]] , | ||
Line 26: | Line 26: | ||
- Windows 10 | - Windows 10 | ||
- | - Download the Inclinometer Design Desktop Application Installer from (link for download) | + | - Download the Inclinometer Design Desktop Application Installer link below |
+ | <WRAP round 80% download> | ||
+ | {{ :resources:eval:user-guides:inertial-mems:accelerometers:inclinometer_design_desktop_application_installer.zip |Inclinometer Design Desktop Application Installer}} | ||
+ | |||
+ | </WRAP> | ||
+ | - Extract the Installer from the Zipped folder. | ||
+ | |||
- Double-click on the Inclinometer Design Desktop Application Installer. | - Double-click on the Inclinometer Design Desktop Application Installer. | ||
Line 188: | Line 194: | ||
**Figure 21:** The Inclinometer Design Desktop Application GUI (Calculated Angle Error Due to Accelerometer Offset) | **Figure 21:** The Inclinometer Design Desktop Application GUI (Calculated Angle Error Due to Accelerometer Offset) | ||
</wrap> | </wrap> | ||
+ | |||
+ | |||
+ | **Reference:** | ||
+ | Fisher, C.(2010).Using an accelerometer for inclination sensing. AN-1057, Application note, Analog Devices | ||
+ |