Wiki

This version (09 Jun 2022 05:40) was approved by Pablo del Corro.The Previously approved version (09 Feb 2022 22:57) is available.Diff

Evaluating the ADXL314

The ADXL314 is a 3-axis accelerometer that provides low power consumption and high-resolution measurement up to ±200 g. The digital output data is formatted as 16-bit, twos complement data and is accessible through a SPI (3- or 4-wire) or I2C digital interface.

Useful links:

ADXL314 Quick Start User Guide:

EVAL-ADXL314-SDP:

The EVAL-ADXL314-SDP drivers and User Guide can be downloaded from the following ftp site: EVAL-ADXLx-SDP Eval Platform.

The EVAL-ADXL314-SDP User Guide wiki: EVAL-ADXL314-SDP User Guide

resources/eval/user-guides/inertial-mems/accelerometers/adxl314.txt · Last modified: 09 Jun 2022 05:40 by Pablo del Corro