This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-ltc4306:no-os-setup [24 May 2023 02:03] – Jose Ramon San Buenaventura | resources:eval:user-guides:eval-ltc4306:no-os-setup [24 May 2023 02:23] (current) – formatting Joyce Velasco | ||
---|---|---|---|
Line 51: | Line 51: | ||
Once the [[ADI> | Once the [[ADI> | ||
- | + | \\ | |
- | < | + | \\ |
- | | Speed | **57600** | | + | For Maxim platforms, the following UART settings are used: |
- | | Data Bits | **8** | + | <WRAP round center 50%> |
- | | Stop Bits | **1** | + | | Speed | **57600** |
- | | Parity | + | | |
- | | Flow Control | **None** | + | | |
- | </note> | + | | |
+ | | | ||
+ | </WRAP> | ||
\\ | \\ | ||
==== ADuCM3029 Platform ==== | ==== ADuCM3029 Platform ==== | ||
Line 70: | Line 72: | ||
== Required Connections == | == Required Connections == | ||
Connect the [[ADI> | Connect the [[ADI> | ||
- | + | \\ | |
- | < | + | \\ |
+ | For [[adi> | ||
+ | <WRAP round center 50%> | ||
| Speed | **115200** | | | Speed | **115200** | | ||
| Data Bits | **8** | | | Data Bits | **8** | | ||
Line 77: | Line 81: | ||
| Parity | | Parity | ||
| Flow Control | **None** | | Flow Control | **None** | ||
- | </note> | + | </WRAP> |
===== No-OS Build Setup ===== | ===== No-OS Build Setup ===== |