Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the EV-COG-AD4050LZ development platform. This software layer is the highest layer of abstraction from the microprocessor, and because of this can be useful to jump start code development for your application using any microprocessor. For example, if you are using the ADXL362, the Sensor software pack contains drivers and code snippets on the application level, so that can be transported to other microprocessor, with confidence that Analog Devices provided the application framework pieces. When combined with the ADuCM4050 and EV-COG-AD4050LZ software packs there are many great Internet of Things(IoT) applications.
ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM4050 Device Family Pack 2.0.0 and EV-COG-AD4050LZ Board Support Package 1.0.0.
The following application examples and sensor drivers are provided as part of the Sensor software pack:
For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide.
ADD LINK HERE Sensor Software Pack Release Notes.
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EC-COG-AD4050LZ platform.
The software pack can be downloaded in following ways.
Download the Sensor Software Pack.
End of Document