Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [31 Jul 2017 15:17]
Pranit Jadhav
resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [11 Aug 2017 16:21] (current)
Pranit Jadhav [General Description/Overview]
Line 2: Line 2:
 ===== General Description/​Overview ===== ===== General Description/​Overview =====
  
-The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI>​ADuCM4050]] devices. ​ This software layer is the foundation layer needed when writing applications using this microprocessor family. ​ When combined with the EV-COG-AD4050LZ software pack as well as the Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD4050LZ development platform.+The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI>​ADuCM4050]] devices. ​ This software layer is the foundation layer needed when writing applications using this microprocessor family. ​ When combined with the **EV-COG-AD4050LZ** software pack as well as the Sensors software pack, there are many great **Internet of Things(IoT)** applications and demos that can be replicated using the **EV-COG-AD4050LZ** development platform.
  
 The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack: The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack:
Line 21: Line 21:
 <WRAP center round help 60%> <WRAP center round help 60%>
  
- ADD DFP RELEASE NOTE LINK HERE + [[http://​download.analog.com/​tools/​EZBoards/​ADuCM4050/​Releases/​DeviceFamilyPack/​Release_1.0.0/​ADuCM4x50_DFP_1.0.0_Release_Notes.pdf | ADuCM4050 ​DFP 1.0.0 Release Notes]]
 </​WRAP>​ </​WRAP>​
  
 <WRAP center round important 60%> <WRAP center round important 60%>
  
-You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD4050LZ platform.+You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the **EV-COG-AD4050LZ** platform.
  
 </​WRAP>​ </​WRAP>​
Line 35: Line 34:
 The software pack can be installed directly by the tool chain'​s CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager'​s manual installation to install the pack. The software pack can be installed directly by the tool chain'​s CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager'​s manual installation to install the pack.
   - Downloaded via the tool chain'​s CMSIS pack manager   - Downloaded via the tool chain'​s CMSIS pack manager
-      * It is **recommended** to download the ADuCM4x50 software pack through from the tool chain'​s CMSIS pack manager. ​ That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. ​ For a detailed description on how to download the ADuCM4x50 software pack through CrossCore Embedded Studio please see our [[resources:​eval:​user-guides:​eval-adicup3029:tools:cces_user_guide#​how_to_install_or_upgrade_the_aducm302x_device_family_pack_dfp_for_cces|CrossCore ​Embedded Studio Quickstart User Guide]].+      * It is **recommended** to download the ADuCM4x50 software pack through from the tool chain'​s CMSIS pack manager. ​ That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. ​ For a detailed description on how to download the ADuCM4x50 software pack through CrossCore Embedded Studio please see our [[resources:​eval:​user-guides:​eval-cog-ad4050lz:tools:cces_guide|Cross Core Embedded Studio Quickstart User Guide]].
   - Downloaded to local directory   - Downloaded to local directory
        * However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to "​import"​ the pack file using your tool chain'​s CMSIS pack manager'​s import feature. Note that all software packs can be downloaded from Keil's website.        * However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to "​import"​ the pack file using your tool chain'​s CMSIS pack manager'​s import feature. Note that all software packs can be downloaded from Keil's website.
Line 41: Line 40:
 <WRAP round 80% download>​ <WRAP round 80% download>​
  
-ADD LNK HERE DFP+[[http://​download.analog.com/​tools/​EZBoards/​ADuCM4050/​Releases/​DeviceFamilyPack/​Release_1.0.0/​ADuCM4x50_Device_Family_Pack-Rel1.0.0.zip | ADuCM4050_DFP Pack 1.0.0]]
    
 </​WRAP>​ </​WRAP>​
  
 // End of Document // // End of Document //
resources/eval/user-guides/eval-cog-ad4050lz/software/aducm4x50.1501507079.txt.gz · Last modified: 31 Jul 2017 15:17 by Pranit Jadhav