This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [31 Jul 2017 15:17] – Pranit Jadhav | resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [31 Jul 2017 15:35] – [Downloading the ADuCM4x50 Software Pack] Pranit Jadhav | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== General Description/ | ===== General Description/ | ||
- | The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI> | + | The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI> |
The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack: | The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack: | ||
Line 27: | Line 27: | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD4050LZ platform. | + | You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the **EV-COG-AD4050LZ** platform. |
</ | </ | ||
Line 35: | Line 35: | ||
The software pack can be installed directly by the tool chain' | The software pack can be installed directly by the tool chain' | ||
- Downloaded via the tool chain' | - Downloaded via the tool chain' | ||
- | * It is **recommended** to download the ADuCM4x50 software pack through from the tool chain' | + | * It is **recommended** to download the ADuCM4x50 software pack through from the tool chain' |
- Downloaded to local directory | - Downloaded to local directory | ||
* However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to " | * However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to " |