Wiki

no way to compare when less than two revisions

Differences

This shows you the differences between two versions of the page.


Previous revision
Next revision
resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4x50 [31 Jul 2017 15:35] – [Downloading the ADuCM4x50 Software Pack] Pranit Jadhav
Line 1: Line 1:
 +====== ADuCM4x50 On-Chip Peripherals Drivers & Software ======
 +===== General Description/Overview =====
  
 +The ADuCM4x50 Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for [[ADI>ADuCM4050]] devices.  This software layer is the foundation layer needed when writing applications using this microprocessor family.  When combined with the **EV-COG-AD4050LZ** software pack as well as the Sensors software pack, there are many great **Internet of Things(IoT)** applications and demos that can be replicated using the **EV-COG-AD4050LZ** development platform.
 +
 +The following on-chip drivers are provided as part of the ADuCM4x50 Device Family Pack:
 +  * spi  {{ :resources:eval:user-guides:eval-cog-ad4050lz:software:aducm4050-fbl.png?600|}}
 +  * i2c
 +  * uart
 +  * sport
 +  * beep
 +  * wdt
 +  * gpio
 +  * rtc
 +  * dma
 +  * crypto
 +  * adc
 +  * tmr
 +
 +For detailed information regarding the ADuCM4x50 DFP, please see our complete ADuCM4x50 software user guide.
 +<WRAP center round help 60%>
 +
 + ADD DFP RELEASE NOTE LINK HERE
 +
 +</WRAP>
 +
 +<WRAP center round important 60%>
 +
 +You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the **EV-COG-AD4050LZ** platform.
 +
 +</WRAP>
 +
 +===== Downloading the ADuCM4x50 Software Pack =====
 +
 +The software pack can be installed directly by the tool chain's CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager's manual installation to install the pack.
 +  - Downloaded via the tool chain's CMSIS pack manager
 +      * It is **recommended** to download the ADuCM4x50 software pack through from the tool chain's CMSIS pack manager.  That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed.  For a detailed description on how to download the ADuCM4x50 software pack through CrossCore Embedded Studio please see our [[resources:eval:user-guides:eval-cog-ad4050lz:tools:cces_guide|Cross Core Embedded Studio Quickstart User Guide]].
 +  - Downloaded to local directory
 +       * However if you do decide to download the ADuCM4x50 software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to "import" the pack file using your tool chain's CMSIS pack manager's import feature. Note that all software packs can be downloaded from Keil's website.
 +
 +<WRAP round 80% download>
 +
 +ADD LNK HERE DFP
 + 
 +</WRAP>
 +
 +// End of Document //
resources/eval/user-guides/eval-cog-ad4050lz/software/aducm4x50.txt · Last modified: 11 Aug 2017 16:21 by Pranit Jadhav