Wiki

This version is outdated by a newer approved version.DiffThis version (11 Aug 2017 13:33) was approved by Pranit Jadhav.

This is an old revision of the document!


EV-COG-AD3029LZ On-Board Peripheral Drivers and Software

General Description/Overview

The EV-COG-AD3029LZ software pack provides access to all the necessary on-board peripheral drivers for the EV-COG-AD3029LZ development platform. This software layer is the secondary layer needed when writing applications using this development platform. The EV-COG-AD3029LZ software pack builds on top of what the ADuCm302x software pack provides. The EV-COG-AD3029LZ software pack makes it easier to use the on-board peripherals so creating your application layer is will be easier. Combined with the ADuCM302x and Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD3029LZ development platform.

The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio 2.6.0 ® and the ADuCM302x Device Family Pack 2.0.0.

EV-COG-AD3029LZ software pack contains the following components:

  • Bluetooth Companion Module
  • On-Chip Driver Examples ( GPIO,RTC, SPI, Systick, TMR, UART, WDT)
  • Bluetooth Profile Examples
    • * FindMe Target
    • * Proximity Reporter
    • * Data Exchange (Hello World)
  • Android IoTNode application software
  • Documentation

For detailed information regarding the EV-COG-AD3029LZ software pack, please see our complete EV-COG-AD3029LZ software user guide.

ADD LINK HERER EV-COG-AD3029LZ BSP Release Notes

You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD3029LZ platform.

Downloading the EV-COG-AD3029LZ Software Pack

The software pack can be downloaded in several ways.

  1. Downloaded via the tools program
    • It is recommended to download the EV-COG-AD3029LZ software pack through from the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the EV-COG-AD3029LZ software pack through CrossCore Embedded Studio please see our CrossCore Embedded Studio Quickstart User Guide.
  2. Downloaded to local directory
    • However if you do decide to download the EV-COG-AD3029LZ software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.

ADD BSP PACK LINK

End of Document

resources/eval/user-guides/eval-cog-ad3029lz/software/ev-cog-ad3029lz.1502432038.txt.gz · Last modified: 11 Aug 2017 08:13 by Pranit Jadhav