This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:eval-cog-ad3029lz:packs_bsp [12 Aug 2017 07:54] Pranit Jadhav |
resources:eval:user-guides:eval-cog-ad3029lz:packs_bsp [12 Aug 2017 08:10] Pranit Jadhav |
||
---|---|---|---|
Line 5: | Line 5: | ||
The Cog software development kit consists of these packs | The Cog software development kit consists of these packs | ||
- | - [[resources:eval:user-guides:eval-cog-ad3029lz:software:aducm302x|DFP- Device Family Pack for ADuCM3029]] - This is a bare minimum pack required to enable working with ADuCM3029 and develop simple applications using the on-chip drivers. | + | - [[resources:eval:user-guides:ev-cog-ad3029lz:software:aducm302x|DFP- Device Family Pack for ADuCM3029]] - This is a bare minimum pack required to enable working with ADuCM3029 and develop simple applications using the on-chip drivers. |
- | - [[resources:eval:user-guides:eval-cog-ad3029lz:software:ev-cog-ad3029lz|BSP - Board Support Package for EV-COG-AD3029LZ]] - This pack along with the DFP is required to develop applications using the on-board drivers. | + | - [[resources:eval:user-guides:ev-cog-ad3029lz:software:ev-cog-ad3029lz|BSP - Board Support Package for EV-COG-AD3029LZ]] - This pack along with the DFP is required to develop applications using the on-board drivers. |
- | - [[resources:eval:user-guides:eval-cog-ad3029lz:software:sensor|SASP - Sensor Application Software Packs]] - This pack is required only to develop applications using the GEARs. Following Sensor Application are included in the pack. | + | - [[resources:eval:user-guides:ev-cog-ad3029lz:software:sensor|SASP - Sensor Application Software Packs]] - This pack is required only to develop applications using the GEARs. Following Sensor Application are included in the pack. |
* Accelerometer Demo | * Accelerometer Demo | ||
* Temperature Sensor Demo | * Temperature Sensor Demo | ||
* Visible Light Sensor Demo | * Visible Light Sensor Demo | ||
- | - [[resources:eval:user-guides:eval-cog-ad3029lz:software:connectivity| Connectivity Packs]] - This pack is required to enable BLE connectivity using EV-COG-BLEINTP1Z connectivity Cog. | + | - [[resources:eval:user-guides:ev-cog-ad3029lz:software:connectivity| Connectivity Packs]] - This pack is required to enable BLE connectivity using EV-COG-BLEINTP1Z connectivity Cog. |
* BLE Pack | * BLE Pack | ||