Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:eval-cog-ad3029lz:packs_bsp [12 Aug 2017 07:54] Pranit Jadhavresources:eval:user-guides:eval-cog-ad3029lz:packs_bsp [12 Aug 2017 08:10] (current) Pranit Jadhav
Line 5: Line 5:
  
 The Cog software development kit consists of these packs The Cog software development kit consists of these packs
-   - [[resources:eval:user-guides:eval-cog-ad3029lz:software:aducm302x|DFP- Device Family Pack for ADuCM3029]] - This is a bare minimum pack required to enable working with ADuCM3029 and develop simple applications using the on-chip drivers. +   - [[resources:eval:user-guides:ev-cog-ad3029lz:software:aducm302x|DFP- Device Family Pack for ADuCM3029]] - This is a bare minimum pack required to enable working with ADuCM3029 and develop simple applications using the on-chip drivers. 
-   - [[resources:eval:user-guides:eval-cog-ad3029lz:software:ev-cog-ad3029lz|BSP - Board Support Package for EV-COG-AD3029LZ]] - This pack along with the DFP is required to develop applications using the on-board drivers. +   - [[resources:eval:user-guides:ev-cog-ad3029lz:software:ev-cog-ad3029lz|BSP - Board Support Package for EV-COG-AD3029LZ]] - This pack along with the DFP is required to develop applications using the on-board drivers. 
-   - [[resources:eval:user-guides:eval-cog-ad3029lz:software:sensor|SASP - Sensor Application Software Packs]] - This pack is required only to develop applications using the GEARs. Following Sensor Application are included in the pack.+   - [[resources:eval:user-guides:ev-cog-ad3029lz:software:sensor|SASP - Sensor Application Software Packs]] - This pack is required only to develop applications using the GEARs. Following Sensor Application are included in the pack.
          * Accelerometer Demo          * Accelerometer Demo
          * Temperature Sensor Demo          * Temperature Sensor Demo
          * Visible Light Sensor Demo          * Visible Light Sensor Demo
-   - [[resources:eval:user-guides:eval-cog-ad3029lz:software:connectivity| Connectivity Packs]] - This pack is required to enable BLE connectivity using EV-COG-BLEINTP1Z connectivity Cog.+   - [[resources:eval:user-guides:ev-cog-ad3029lz:software:connectivity| Connectivity Packs]] - This pack is required to enable BLE connectivity using EV-COG-BLEINTP1Z connectivity Cog.
         * BLE Pack         * BLE Pack
  
resources/eval/user-guides/eval-cog-ad3029lz/packs_bsp.txt · Last modified: 12 Aug 2017 08:10 by Pranit Jadhav